Skip to main content
eyals111
Associate II
Feb 4, 2014 3:16 PM UTC
Solved

M24SR - mistake in table 67 Datasheet

Posted on February 04, 2014 at 16:16

hi , 

1.i have been playing with M24SR16-Y for few days , just  want to inform that there is a     mistake in table 67 .

  the Payload written in table 67  :   00 A4 00 07 02 D2 76 00 00 85 01 01

  should Be                                   :   00 A4 04 00 07 D2 76 00 00 85 01 01 00 (According                                                    to Chapter 5.6.3 , also checked with the IC return 90 00.)

the CRC  matched to the Correct Payload (including the PCB  byte = 0x02 Or 0x03)

#crc #m24sr
This topic has been closed for replies.
Anais GALLIGANI
Anais GALLIGANIBest answer
Visitor II
Feb 10, 2014 3:32 PM UTC
Posted on February 10, 2014 at 16:32

Hi,

Thanks for the note,

It will be corrected in the next revision,

Have a nice day,

ST NFC/RFID Dynamic tag support

1 reply

Anais GALLIGANI
Anais GALLIGANIBest answer
Visitor II
Feb 10, 2014 3:32 PM UTC
Posted on February 10, 2014 at 16:32

Hi,

Thanks for the note,

It will be corrected in the next revision,

Have a nice day,

ST NFC/RFID Dynamic tag support