Skip to main content
Visitor
Oct 22, 2026 6:33 AM UTC
Solved

M24LR64E-RDW6T/2 - RFID memory code changed from C to D - Req confirmation

Hi STMicro team,

On usage of MPN:M24LR64E-RDW6T/2, recent datecode: 102026 (WWYYYY)  , we find below difference:

The difference is  C to D change in the chip RFID module :

Old Build Board

  • RFID Memory Code: E0025C9196D23D96
  • Date Code: 2336
  • Result: 100% Pass Rate

New Build Board

  • RFID Memory Code: E0025D71B0C4273
  • Date Code: 2610
  • Result: Boards Failed During FCT (100%)

 

The customer has requested clarification regarding the change from "C" to "D" in the RFID memory code,.

Could you please check with the supplier / STMicroelectronics and confirm the following:

  1. Is this only a product code/marking change?
  2. Is there any change in component characteristics, specifications, firmware, or functionality compared to the previous build?
JL. Lebon
JL. LebonBest answer
ST Employee
Oct 22, 2026 8:06 AM UTC

Hello, 

The UID of the device is a unique serial number that is incremented while devices are produced.
So, the difference of value you see here is just telling us that the “D” devices have been produced more recently than the “C” devices.

There is no change in the component characteristics or specification between the two devices you are referencing. They are the same device.

If you have failures on a specific production lot, you should contact your local ST sales. They will put you in contact with the right people in charge of quality, who are qualified to handle this kind of request. Please find contacts here: Contacts - STMicroelectronics

Best regards.

1 reply

JL. Lebon
JL. LebonBest answer
ST Employee
Oct 22, 2026 8:06 AM UTC

Hello, 

The UID of the device is a unique serial number that is incremented while devices are produced.
So, the difference of value you see here is just telling us that the “D” devices have been produced more recently than the “C” devices.

There is no change in the component characteristics or specification between the two devices you are referencing. They are the same device.

If you have failures on a specific production lot, you should contact your local ST sales. They will put you in contact with the right people in charge of quality, who are qualified to handle this kind of request. Please find contacts here: Contacts - STMicroelectronics

Best regards.