Skip to main content
muralik
Visitor II
Mar 6, 2014 1:50 PM UTC
Solved

m24lr64e first time programming/ reading

Posted on March 06, 2014 at 14:50

Hi,

We have a custom board made using M64LR64E. Using an android phone, without powering up, will the EEPROM work directly as a NFC tag? Or should it be programmed/ configured first using I2C?

We are unable to detect as NFC Tag. We are using smd inductor for antenna and don't have 4.7uH inductors presently and are using a 6.8uH. Is this the reason why it is not working?

How do you check the functioning of the memory over RF for the first time?

Thanks

Murali

#m24lr #m24lr #rf #inductor #memory #antenna
This topic has been closed for replies.
Anais GALLIGANI
Anais GALLIGANIBest answer
Visitor II
Mar 10, 2014 9:41 AM UTC
Posted on March 10, 2014 at 10:41

Hello,

Yes you need 4.7 µH.

Because with the internal capacitance, it allows to get the right frequency in order to communicate with the reader or smartphone.

Please use a 4.7 µH antenna.

Thanks,

Have a nice day,

ST NFC/RFID Dynamic tag e2e support

1 reply

Anais GALLIGANI
Anais GALLIGANIBest answer
Visitor II
Mar 10, 2014 9:41 AM UTC
Posted on March 10, 2014 at 10:41

Hello,

Yes you need 4.7 µH.

Because with the internal capacitance, it allows to get the right frequency in order to communicate with the reader or smartphone.

Please use a 4.7 µH antenna.

Thanks,

Have a nice day,

ST NFC/RFID Dynamic tag e2e support