Skip to main content
jourjon
Visitor II
June 6, 2014
Solved

M24LR16E Incompatibility with Smartphones (S4/Nexus 4...)

Posted on June 06, 2014 at 05:47

Hi all,

I am using a ST NFC chip : M24LR16E in my products and I noticed some incompatibility with Smartphones of the market (Samsung S4, S5, Nexus 4)

I have made some research and I found that these phones were using a Broadcom NFC chip (BC20794) which is not compatible with some NFC chips in the product. It depends on the type of NFC tag used. (Most of existing products has Mifare Classic 1k tag and it is just compatible with NXP chip equiped phones). 

In fact the M24LR16E has ISO15693 standard, which is the same standard as in the NXP NFC chips of the Smartphones (PN544, PN65N...). Whereas the ISO standards in the Broadcom chips are ISO 18092, ISO14443 (from NFC Forum type 1-4 tags)...

So the problems comes from this different type of NFC tags technology (Mifare Classic 1k vs NFC Forum Type 1-4)? Or is it coming from the application?

Do someone has the same problems? Do we need to change the M24LR16E chips?

Thank you for your answers

Regards

#nfc #compatible #mifare #iso15693 #m24lr16e #m24sr #m24lr #nfc
This topic has been closed for replies.
NFC/RFID Customer support
ST Employee
June 30, 2015
Posted on June 30, 2015 at 15:29

Hi,

I suppose you are using M24LR-Discovery and want to read the temperature value (displayed on LCD screen) with RF path. Unfortunately, the temperature value is not stored in the M24LR04E by the firmware and so, cannot be read by RF. The temperature value is directly read and displayed at screen by the microcontroler. To be able to read temperature through RF, you should modify the firmware code in order to read the temperature via microcontroler , then write temperature value in the M24LR04E. After this modifications, the temperature value will be available via RF.

This is source code of the M24LR-Discovery STM8L microcontroler:

http://www.st.com/web/en/catalog/tools/PF258104

To read M24LR04E through CR95HF, you can use M24LR_Application_Software .

http://www.st.com/web/en/catalog/tools/PF257516

Best regards,

NFC/RFID ST support

4 replies

Anais GALLIGANI
Visitor II
August 28, 2014
Posted on August 28, 2014 at 15:22

Hello,

M24LR16E is a dynamic tag ISO 15693, that can be support per

- All ISO 15693 reader/writer (from ST and competition)

- Most NFC smartphone (Android +BB10)

The M24LR embeds also specific functions that is not defined as standard (this is also the case of most ISO 15693 tags market offering differentiating functions) . For M24LR : high density addressing mode, energy harvesting, password…

And through the embedded software of the industrial reader, it will be possible to handle specific functions of each tag (need firmware update)

And we have in our portfolio also the M24SR dynamic tag : ISO 14443 , compliant with all NFC smartphone.

http://www.st.com/m24sr

M24LR & M24SR are pin to pin compatible.

Have a nice day,

ST NFC RFID dynamic tag support
yanfeng
Visitor II
April 28, 2015
Posted on April 28, 2015 at 12:22

Sorry,i am trying to get the temperature of M24LR04E tag. How can i get the current temperature via CR95HFDLL?

NFC/RFID Customer support
ST Employee
June 30, 2015
Posted on June 30, 2015 at 15:29

Hi,

I suppose you are using M24LR-Discovery and want to read the temperature value (displayed on LCD screen) with RF path. Unfortunately, the temperature value is not stored in the M24LR04E by the firmware and so, cannot be read by RF. The temperature value is directly read and displayed at screen by the microcontroler. To be able to read temperature through RF, you should modify the firmware code in order to read the temperature via microcontroler , then write temperature value in the M24LR04E. After this modifications, the temperature value will be available via RF.

This is source code of the M24LR-Discovery STM8L microcontroler:

http://www.st.com/web/en/catalog/tools/PF258104

To read M24LR04E through CR95HF, you can use M24LR_Application_Software .

http://www.st.com/web/en/catalog/tools/PF257516

Best regards,

NFC/RFID ST support

anthonyanthony9
Associate II
April 20, 2016
Posted on April 20, 2016 at 19:10

Hi,

I too plan to use the M24LR to interface with an NFC enabled android phone (thought the M24LR Discovery) . The main appeal being the device will not require batteries. however I am now concerned about compatibility issues outlined here. Can the M24SR simply be soldered inplace of the M24LR on the discovery board whiles maintaining all functionality (particularly the energy harvesting and bidirectional data flow)

Alternately does ST have an M24SR discovery board available which utilises energy harvesting