Skip to main content
dkilshtein9
Associate III
May 4, 2015 8:15 AM UTC
Solved

M24LR-DISCOVERY question

Posted on May 04, 2015 at 10:15

Hi

I need to store a single file on the board from a PC (with ST application via USB) then I need to be able to read the file back to the PC (with ST application via USB). In addition, I need to be able to transfer the same file (via NFC) to any reader (i.e. smart phone)

I have only the ''RF transceiver board'' that is connected to the PC with USB.

I downloaded the demo application for it (stsw-m24lr011) but I can't make it communicate with the board via USB. Is there a way to store file on this board at all and if so, hot to accomplish this task?

Thanks a lot.

#nfc
This topic has been closed for replies.
NFC/RFID Customer support
ST Employee
Jun 30, 2015 1:39 PM UTC
Posted on June 30, 2015 at 15:39

Hi,

you can use M24LR11 (M24LR_Application_Software) to communicate with M24LR-Discovery. You can use ''show Demo NDEF & Energy Harvesting'' demo to communicate with M24LR-Discovery board (using NDEF message). Anyway you can download any king of data (4Kbit max) in M24LR04E using ''Reader Application'' menu selecting M24LR04E product.

Best regards,

NFC/RFID ST support

1 reply

NFC/RFID Customer support
ST Employee
Jun 30, 2015 1:39 PM UTC
Posted on June 30, 2015 at 15:39

Hi,

you can use M24LR11 (M24LR_Application_Software) to communicate with M24LR-Discovery. You can use ''show Demo NDEF & Energy Harvesting'' demo to communicate with M24LR-Discovery board (using NDEF message). Anyway you can download any king of data (4Kbit max) in M24LR04E using ''Reader Application'' menu selecting M24LR04E product.

Best regards,

NFC/RFID ST support