Skip to main content
kolwas
Associate II
November 17, 2022
Solved

Low power read

Hello,

I need to make ST25R3916 read as power efficient as possible. I am searching for documentation, but only this voltage regulator I see (0x2C). Is there any option to change field power of NFC to make a read as power efficient as possible? NFC tag will be always on fixed position in fixed range.

Important: we are not talking about detecting card - as capacitance detection is good enough but only on reading the card

This topic has been closed for replies.
Ulysses HERNIOSUS
ST Technical Moderator
November 22, 2022

Hi,

I don't understand your comments on "10% max".

I you want to reduce output power you can play with d_res settings. Inside analogConfigTbl_NFC06A1.c this would be this line here:

0x0028,0x0f,0x00, /* RFO driver resistance Active transmission (d_res) ; Set RFO resistance Active Tx */

Alternatively you could also try to manually set the voltage regulator by adding a line to set the regulator to a low level:

0x002c,0xf8,0x80, /* reg_s=1, manual set to 3.6V */

BR, Ulysses

3 replies

Travis Palmer
ST Employee
November 17, 2022

Hello Kolwas,

There are many screws to adjust the output power.

First would be the antenna geometry.

The antenna should be designed in a way, that you have the best coupling in the desired distance.

Also the Q-factor should be properly adjusted to the desired technology and bit rate.

Once done, the best chance to adjust the output power is to select a proper matching impedance.

All information about the above mentioned facts can be found in AN5276.

Since the read range is dependent on reader antenna, tag antenna and coupling, a clear link between read range and matching impedance cannot be done - you will simply have to do try and error to minimize the read range.

br Travis

kolwas
kolwasAuthor
Associate II
November 18, 2022

I use NFC06A1 board where the settings are tuned but still, it's 500mA. I need to decrease. I changed max bound rate and no change on current. I use ST ST25NFC_Embedded_Lib_ST25R3916_1.4.0, and all settings are changing game on 10% max, so there are very restricted for me.

Could you please give me a hint how to change from software perspective? To just decrease the max NFC field power?

Ulysses HERNIOSUS
ST Technical Moderator
November 22, 2022

Hi,

I don't understand your comments on "10% max".

I you want to reduce output power you can play with d_res settings. Inside analogConfigTbl_NFC06A1.c this would be this line here:

0x0028,0x0f,0x00, /* RFO driver resistance Active transmission (d_res) ; Set RFO resistance Active Tx */

Alternatively you could also try to manually set the voltage regulator by adding a line to set the regulator to a low level:

0x002c,0xf8,0x80, /* reg_s=1, manual set to 3.6V */

BR, Ulysses