Skip to main content
DGrgic
Associate
December 17, 2020
Solved

Low power mode ST25R95, power consumption?

Hello,

I'm using ST25R95 in my project. I'm sending pulse signal in order to transit from powerUP mode, and after it the Idle command in order to enter hibernate mode.

Idle command: {0x07, 0x0E, 0x08, 0x04, 0x00, 0x04, 0x00, 0x18, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00};

I'm using custom PCB and current consumption after I send Idle command drops from 1.69mA to 1.14mA.

The rest of circuit on the PCB consumes 0.14mA, which means there is about 1mA current somewhere in the NFC circuit.

In the DB2382 Rev 5 document, I have found reference design for the ST25R95, and SSI_0 is connected over 3.3kOhms to VCC, and SSI_1 over 3.3kOhms to GND. That is the only difference from mine design, because I have connected those 2 pins directly to VCC and GND respectively (SSI_0 to VCC, and SSI_1 to GND). Could this be an issue and is that reason for this 1mA power consumption, or do I need to do something else besides sending the Idle command?

Best regards and thank you in advance,

Dragan

    This topic has been closed for replies.
    Ulysses HERNIOSUS
    ST Technical Moderator
    December 23, 2020

    Hi Dragan,

    the response to Idle command can only be read once IRQ_OUT went low. Please refer to Table 24 in DS.

    Regards, Ulysses

    3 replies

    Brian TIDAL
    ST Technical Moderator
    December 18, 2020

    Hi @DGrgic​ 

    the Idle command seems correct.

    I would suggest to compare your schematics with the X-NUCLEO-NFC03 ones (see UM2479 for the schematics) and use the same pull up/down resistors. You can first measure the current consumption on X-NUCLEO-NFC03 in case of any doubts.

    Also, please make sure to rely on IRQ_OUT before reading the answer to the Idle command (i.e. SPI poll cannot be used while in low power and Application has to rely on IRQ_OUT, see Datasheet §5.9)

    Rgds

    BT

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    DGrgic
    DGrgicAuthor
    Associate
    December 19, 2020

    Hello @Brian TIDAL_O​ ,

    Thank you for your response.

    After we send the Idle command, the IRQ_OUT pin remains in a HIGH state, so we don't try to read the response with SPI.

    If the device is sent in hibernate mode, using the Idle command is it supposed to answer?

    Ulysses HERNIOSUS
    ST Technical Moderator
    December 23, 2020

    Hi Dragan,

    the response to Idle command can only be read once IRQ_OUT went low. Please refer to Table 24 in DS.

    Regards, Ulysses