Skip to main content
MikeObs
Associate II
November 2, 2020
Solved

Looking for smart cards working on different standards. Anybody have an idea where can I find those?

I have been working on a project with CR95HF multi-protocol transceiver IC. The obvious advantage of it is that it can read tags working with different protocols (different standards).

I already coded so the IC reads different standards according to the datasheet but all I need now is to test the functionality. I have a Mifare classic tag at home, but I would like to test 14443B, 15693 and 18092 tags. Any idea where can I find a set of tags all working on a different standards? All I need is couple read only cards where I can read a UID of them (possibly having a UID written on the to see if the reading is correct) so I can see if my algorithms are coded correctly. Any idea where can I buy a cards like this or if I can somehow obtain them from someone?? Thanks a lot for the help!

    This topic has been closed for replies.
    Brian TIDAL
    Brian TIDALBest answer
    ST Technical Moderator
    November 2, 2020

    Hi,

    • For ISO/IEC 15693 tags, you can use ski passes from almost any ski resort. You can also purchase an M24LR-DISCOVERY kit where an ISO/IEC 15693 tag is available, or a ST25DV-PWM-eSET or a ST25DV-DISCOVERY kit.
    • For 18092, you can use Android NFC smartphone (most of them emulate both ISO/IEC 14443-A and 18092 tags).
    • For ISO/IEC 14443-B, you can use a bio-metric passport.

    Rgds

    BT

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

    3 replies

    Brian TIDAL
    Brian TIDALBest answer
    ST Technical Moderator
    November 2, 2020

    Hi,

    • For ISO/IEC 15693 tags, you can use ski passes from almost any ski resort. You can also purchase an M24LR-DISCOVERY kit where an ISO/IEC 15693 tag is available, or a ST25DV-PWM-eSET or a ST25DV-DISCOVERY kit.
    • For 18092, you can use Android NFC smartphone (most of them emulate both ISO/IEC 14443-A and 18092 tags).
    • For ISO/IEC 14443-B, you can use a bio-metric passport.

    Rgds

    BT

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    MikeObs
    MikeObsAuthor
    Associate II
    November 3, 2020

    Hey, thank you for the quick reply!

    I've looked into what you recommended me and have a couple more quick question on you.

    • In the data sheet of CR95HF, you state: ISO/IEC 15693 tags, NFC Forum tags: Types 1, 2, 3 and 4. The board you recommended me (ST25DV-PWM-eSET) has in datasheet stated: Based on ISO/IEC 15693 and NFC Forum Type 5. Of course I believe you, when you said it will work, that it will actually work but my question is why in the CR95HF there is not mentioned NFC forum tag 5 is also supported?
    • I also found ST25TV-eSEAL discovery board, where is stated is also based on ISO/IEC 15693. I assume that will also work, but just making sure if it will.

    Thank you so much for your recommendations for 18092 and 14443B! I will be trying them out soon! You helped me a lot!

    Regards,

    Michal

    Brian TIDAL
    ST Technical Moderator
    November 3, 2020

    Hi,

    I would suggest to use ST25R95 datasheet which contains the most up to date information regarding the ST25R95/CR95HF transceiver:

    Typical protocols supported:

    • ISO/IEC 14443-3 Type A and B tags
    • ISO/IEC 15693 tags
    • ISO/IEC 18000-3M1 tags
    • NFC Forum tags: Types 1, 2, 3, 4 and 5

    To make a long story short on Standards:

    • Based on ISO/IEC 14443-3 Type A , 3 types of tags are defined: T1, T2 and T4-A
    • based on ISO/IEC 14443-3 Type B, one type of tag is defined: T4-B
    • based on ISO/IEC 18000- (aka Felica), one type of tag is defined: T3
    • based on ISO/IEC 15693: one type of tag is defined: T5

    Both ST25DV-PWM-eSET or  ST25DV-DISCOVER or ST25TV-eSEAL work perfectly with ST25R95/CR95HF.

    Rgds

    BT

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.