Skip to main content
ottavio
Associate
Aug 22, 2013 7:03 AM UTC
Solved

Linux driver for the CR95HF-based board

Posted on August 22, 2013 at 09:03

Hello, I am trying to make my m24lr discovery board work under Linux.

I've seen that ST provides a DLL to communicate with the green board under windows, but I'd like to use it under Linux. As far as I've seen, it is a HID device, but even by reading the source codice for its microcontroller, I've been only able to understand that the firmware forwards the commands to the CR95HF, but I was not able to understand the format of the commands.

Do you have a working code to use that board under linux? Or do you have a bit more documentation, so that I can try to use the board with libusb?

Thank you

Ottavio

#cr95hf #linux-driver-cr95hf #linux #linux-driver-cr95hf
This topic has been closed for replies.
Rene Lenerve
Rene LenerveBest answer
ST Employee
Nov 13, 2015 1:44 PM UTC
Posted on November 13, 2015 at 14:44

Hello,

The source files are located in the

STSW-95HF004 web site on st.com, here below you will find the link:

http://www.st.com/web/en/catalog/tools/FM147/SC1871/PF262137?s_searchtype=keyword

#

I hope this can be helpful,

Have a nice day.

8 replies

Anais GALLIGANI
Visitor II
Aug 23, 2013 7:13 AM UTC
Posted on August 23, 2013 at 09:13

Hello,

Might you please send me your email adress in order to help you further?

In a first time this AN might help you :  

AN3954: Developing your own Visual Basic or C/C++ application on a DEMO-CR95HF-A demonstration board

http://www.st.com/st-web-ui/static/active/en/resource/technical/document/application_note/DM00034558.pdf

Have a nice day,

All the best ,

ST NFC/RFID dynamic tag

ottavio
ottavioAuthor
Associate
Aug 29, 2013 7:41 AM UTC
Posted on August 29, 2013 at 09:41

My address is ottavio at campana.vi.it

I already studied the document you're mentioning, but my problem is that I'd like to attach the green board to an arm-based linux system, thus I need to understand how I can make the reader work with linux.

charles2
Visitor II
Dec 11, 2013 12:46 PM UTC
Posted on December 11, 2013 at 13:46

Hello,

I also need to get this M24LR discovery kit working on a linux system. Right now, I use you dll on a windows based PC, but the next step is to move it across to an arm based linux micro-computer. Do you have a linux driver equivalent to the widows dll? My email address, if you need it is charles.whitmore at btinternet.com

thanks & regards

  Charles 

Denis Krasutski
Associate III
Mar 3, 2015 9:02 PM UTC
Posted on March 03, 2015 at 22:02

Hello,

I also need information about communication protocol between MB1054A and HID (I am using Linux,

I do not have

the ability to use

DLL library)

my email: denis.krasutsk(d_o_g)cedoni.com

Best Regards,

Krasutski Denis.
Denis Krasutski
Associate III
Mar 4, 2015 11:51 PM UTC
Posted on March 05, 2015 at 00:51

Sorry, I made a mistake in my email:  denis_krasutski@cedoni.com

Anais GALLIGANI
Visitor II
Jun 26, 2015 2:05 PM UTC
Posted on June 26, 2015 at 16:05

Hello Denis ,

is this helping you also?

http://www.st.com/st-web-ui/static/active/en/resource/technical/document/application_note/DM00134778.pdf?s_searchtype=keyword

Have a nice day,

ST NFC/RFID Support

timo2
Visitor II
Aug 18, 2015 4:03 PM UTC
Posted on August 18, 2015 at 18:03

Hello,

same thing here. The App-Note ''AN4593'' looks great. But where do I find the actual Library files mentioned? Or did I missed something?

I would appreciate if you can send me the required files.

Mail:  Timo.Goestenkors at fh-bielefeld.de

Best regards

Rene Lenerve
Rene LenerveBest answer
ST Employee
Nov 13, 2015 1:44 PM UTC
Posted on November 13, 2015 at 14:44

Hello,

The source files are located in the

STSW-95HF004 web site on st.com, here below you will find the link:

http://www.st.com/web/en/catalog/tools/FM147/SC1871/PF262137?s_searchtype=keyword

#

I hope this can be helpful,

Have a nice day.