Skip to main content
DAbba
Associate II
August 13, 2018
Solved

is ST25 support DESFIRE ?

Hi everyone

I have chosen st25r3911b to my new project for NFC and mifares .

now I am wondering if it dose not support DESfire , I have to change my project and choose another chip .

could you please help me .

This topic has been closed for replies.
Ulysses HERNIOSUS
ST Technical Moderator
August 16, 2018

Hi Darius,

of course ST25R3911B supports sending/receiving all the frames and APDUs need for Mifare Desfire and even Mifare Classic.

AFAIK the full details of the commands etc. are only available under NDA with NXP. So our demo code does not have extensive support for these tags. Our source code will discover, anticollide and activate those cards but no support of cryptography/read/write/format is included. There is sample code inside XNUCLEO-NF05A1 for reading NFC Forum T4T. Mifare DesFire can be formatted as a T4T.

Regards, Ulysses

1 reply

Ulysses HERNIOSUS
ST Technical Moderator
August 16, 2018

Hi Darius,

of course ST25R3911B supports sending/receiving all the frames and APDUs need for Mifare Desfire and even Mifare Classic.

AFAIK the full details of the commands etc. are only available under NDA with NXP. So our demo code does not have extensive support for these tags. Our source code will discover, anticollide and activate those cards but no support of cryptography/read/write/format is included. There is sample code inside XNUCLEO-NF05A1 for reading NFC Forum T4T. Mifare DesFire can be formatted as a T4T.

Regards, Ulysses