Skip to main content
val_ltd
Associate III
Dec 3, 2013 1:02 PM UTC
Solved

Is possible to use M24LR04E for sending NDEF messages?

Posted on December 03, 2013 at 14:02

Hello,

Is possible to use M24LR04E for sending a NDEF message? (intended to read it from a mobile, for making pairing operations, etc..)

Please, is there any example of code, about how publishing an NDEF message in the antenna, using I2C bus?

If not.... please, why not? and what kind of chip could I use?

Is M24SR02-Y chip the right one? I read that it is still on evaluation process... and not for sale.

Thanks in advance,

#m24sr #ndef #ndef #m24lr04e #m24sr02 #m24sr64 #m24lr #m24sr64 #m24sr
This topic has been closed for replies.
Anais GALLIGANI
Anais GALLIGANIBest answer
Visitor II
Dec 10, 2013 9:42 AM UTC
Posted on December 10, 2013 at 10:42

Hello,

Yes it is possible to use M24LR04E for sending a NDEF message

 (intended to read it from a mobile, for making pairing operations, etc..)

You have an application note that explains how to do it.

http://www.st.com/st-web-ui/static/active/en/resource/technical/document/application_note/DM00029842.pdf

With

  • M24LR : ISO 15693 , some smartphones as Galaxy S4 support natively the NDEF inside the M24LR so you dont need to develop any application. With most of ISO 15693 compatible phones, you need to develop an application.

            We provide the source code of our application : NfcV-Reader available on Google play : 

                

http://www.st.com/web/en/catalog/tools/PF257517

  • M24SR : ISO 14443, NFC phones will be able to read the NDEF messages natively.

You can place sample order through disty.

I hope this is helping,

Have a nice day,

ST NFC/RFID Dynamic tag support

From: ramirez_prieto.valen

Posted: Tuesday, December 03, 2013 2:07 PM

Subject: Is possible to use M24LR04E for sending NDEF messages?

Hello,

Is possible to use M24LR04E for sending a NDEF message? (intended to read it from a mobile, for making pairing operations, etc..)

Please, is there any example of code, about how publishing an NDEF message in the antenna, using I2C bus?

If not.... please, why not? and what kind of chip could I use?

Is M24SR02-Y chip the right one? I read that it is still on evaluation process... and not for sale.

Thanks in advance,

11 replies

Anais GALLIGANI
Visitor II
Feb 18, 2014 2:24 PM UTC
Posted on February 18, 2014 at 15:24

Hello ,

Some application notes on this subject will be soon released.

Thanks a lot,

Have a nice day,

Best Regards,

ST NFC/RFID Dynamic tag support