Skip to main content
SS1
Associate II
February 12, 2020
Solved

Interfacing ST25RU3993 with TI micro-controller

Hi,

I have purchased ST25RU3993-EVAL board with complete set and I am able to read tags. I would like to know if I can interface this board - RFID Reader with another micro controller (I wanted to interface with TI CC1352P1 launchpad), via SPI (or via any serial communication). If so is there any programming tool?

Is it possible to obtain driver and library files for ST25RU3993-EVAL board

Thanks in Advance

    This topic has been closed for replies.
    Ulysses HERNIOSUS
    ST Technical Moderator
    February 12, 2020

    Hi,

    I just downloaded the stsw-st25ru003 and it contains all the firmware sources - no Altium Files.

    Regards, Ulysses

    4 replies

    Ozone
    Principal
    February 12, 2020

    There seems to be a SDK, with source code for a STM32L4:

    https://www.st.com/content/st_com/en/products/embedded-software/st25-nfc-rfid-software/stsw-st25ru003.html

    Pretty sure ST will not provide support for other vendor's MCUs.

    SS1
    SS1Author
    Associate II
    February 12, 2020

    Hey, Thanks for the reply!

    But this is not answer I am expecting. I have already installed the firmware and I can also read my Tags. And the source files which are included deals with hardware editing stuffs (with Altium Designer). My question is if there is availability of software driver or library file, I could do programming to interface to another micro controller.

    Kindly help!

    Ulysses HERNIOSUS
    ST Technical Moderator
    February 12, 2020

    Hi,

    I just downloaded the stsw-st25ru003 and it contains all the firmware sources - no Altium Files.

    Regards, Ulysses