Skip to main content
Associate II
April 15, 2025
Solved

Integrating RFAL Files for NFC Communication with STM32Cube

I am currently working on a project that involves reading NFC tags using the NFC X-NUCLEO-NFC08A1 extension, which utilizes the ST25R3916 NFC reader connected to an STM32 Nucleo-G0B1RE platform.

Having completed the hardware interfacing for SPI communication between the two, I have now integrated the RFAL files into the project via the X-CUBE-NFC6 package to enable communication between the STM32Cube software and the NFC reader.

Are there any modifications required in these files to adapt them to the project? Additionally, what is the difference between X-CUBE-NFC6 and STSW-ST25RFAL002?

This topic has been closed for replies.
Brian TIDAL
Brian TIDALBest answer
ST Technical Moderator
April 25, 2025

Hi,

I guess the eclipse editor is not able to find symbols that are defined outside .c or .h files.

Regarding your initial issue with st25r3916CheckChipID, if the ID value returned in st25r3916ReadRegister( ST25R3916_REG_IC_IDENTITY, &ID ); is incorrect (not the one for ST25R3916 nor the one for ST25R3916B), this means the SPI configuration is incorrect or the expansion board is incorrectly plugged-in. See figure 22 in the STMicroelectronics.X-CUBE-NFC6_GettingStarted.pdf for a proper setting of the SPI. Connect a logic analyzer on the SPI pins to check the communication.

Rgds

BT

 

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

7 replies

Brian TIDAL
ST Technical Moderator
April 15, 2025

Hi,

STSW-ST25RFAL002 contains the standalone RFAL only whereas X-CUBE-NFC6 contains full demos (polling demo and NDEF demo) in addition to the RFAL.

When using the X-CUBE-NFC6 with STM32CubeMX, a running project is generated (either based on the polling demo or based on the NDEF demo). It should run out of the box on your board without any modification (make sure to follow the getting started guide inside the documentation folder). Then you can modify the  demo_polling.c file to adapt the application to your own needs.

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate II
April 16, 2025

Thank you so much for your response, it was very helpful. Now, I am encountering an issue with the hardware configuration before generating the code in STM32CubeMX.

I have configured SPI1 under the <connectivity> section, selecting all the appropriate pins for the corresponding signals according to the datasheet and schematic. However, when configuring X-CUBE-NFC6 in the <platform Settings> section, I cannot find the pins I configured for the NFC CS PIN and NFC INT PIN, even though the pins are correctly highlighted in green in the graphical interface.

Brian TIDAL
ST Technical Moderator
April 16, 2025

Hi,

as shown in figure 20 of the STMicroelectronics.X-CUBE-NFC6_GettingStarted.pdf, the hardware NSS signal should be disabled. The SPI1_NSS should be enabled as a GPIO_Output pin (Figure 21).

The NFC INT PIN should be enabled as an EXTI with External Interrupt Mode with Rising edge trigger detection (should not be not a GPIO_input). The related EXTI interrupt should enabled and the interrupt priority must lower than the systick interrupt (lower priority means higher numerical value). Figure 23 shows an incorrect priority for the EXTI Line 0 (should be > 0).

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate II
April 24, 2025

While debugging step-by-step, I noticed that the execution stops at the following point:

In the file `ST25R3916.c`:
if( !st25r3916CheckChipID( NULL ) )
{
platformErrorHandle();
return RFAL_ERR_HW_MISMATCH;

The `platformErrorHandle()` function is defined in `rfal_platform.h` as:
#define platformErrorHandle() _Error_Handler(__FILE__,__LINE__)

And the `_Error_Handler` function is defined as:
void _Error_Handler(char * file, int line)
{
/* USER CODE BEGIN Error_Handler_Debug */
/* User can add his own implementation to report the HAL error return state */
while (1)
{
}
/* USER CODE END Error_Handler_Debug */
}

What could be the issue causing the chip not to be detected? I believe I configured the SPI correctly.

Ulysses HERNIOSUS
ST Technical Moderator
April 24, 2025

Hi,

believing is one thing. Verifying the other. Or to say it with my favorite book: "Quit thinking and look!":

Connect a scope/logic analyzer and see the real sequence. Then you can decide which line is potentially not correctly toggling. Or see an incorrect frequency, ......

Ulysses

Associate II
April 25, 2025

When I Ctrl+click on ST25R3916B, I get the message "Could not find symbol 'ST25R3916B' in index." However, the macro ST25R3916B is correctly defined when I check under MCU GCC Compiler > Preprocessor.

Brian TIDAL
Brian TIDALBest answer
ST Technical Moderator
April 25, 2025

Hi,

I guess the eclipse editor is not able to find symbols that are defined outside .c or .h files.

Regarding your initial issue with st25r3916CheckChipID, if the ID value returned in st25r3916ReadRegister( ST25R3916_REG_IC_IDENTITY, &ID ); is incorrect (not the one for ST25R3916 nor the one for ST25R3916B), this means the SPI configuration is incorrect or the expansion board is incorrectly plugged-in. See figure 22 in the STMicroelectronics.X-CUBE-NFC6_GettingStarted.pdf for a proper setting of the SPI. Connect a logic analyzer on the SPI pins to check the communication.

Rgds

BT

 

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.