Skip to main content
Associate II
November 24, 2025
Solved

I2C and GPO pin max input voltage

I am using ST25DV04KC tag and using the V_EH pin to power the VCC of the tag only( It will generate around 3.3V which is enough to power up the tag in I2C mode I believe) . I am looking for guidance on the maximum pullup voltage on the I2C and GPO line from an external rail of around 3.6V, if it is okay? what can be the max voltage on the I2C and GPO pins? is it independent of VCC or dependent on VCC?

This topic has been closed for replies.
JL. Lebon
JL. LebonBest answer
ST Employee
November 24, 2025

Hello, 

The voltage put on pull-up resistors on the I2C pins and on the GPO pin can be different than the voltage on the VCC pin (I2C and GPO are true open drain pins). This is off course if you are using the open drain version of the GPO pin (ST25DV04K-IE, not -JF version).

The maximum voltage indicated in the maximum rating table in the datasheet (-0.5 to 6.5V) indicates the max that you can reach before damaging the device. Nevertheless, it is not recommended to operate the device at 6.5V.

The recommended operating values are described in the "I2C operating conditions" table and specifies that the voltage should be between 1.8 and 5.5V.

So, you can have a VCC of 3.3V and have pull-ups resistors on GPO and SCL/SDA between 3.3V and 5.5V (you can't go below VCC since the VIH min is 0.75xVCC).

Best regards.

5 replies

gbm
Super User
November 24, 2025

Read The Fine Datasheet - you should find the relevant information there.

My STM32 stuff on github - compact USB device stack and more: https://github.com/gbm-ii/gbmUSBdevice
MagvelAuthor
Associate II
November 24, 2025

I went through the datasheet, found the max voltage rating for I2C and GPO is given as -0.5 to 6.5 Volt. There is no mention of the VCC voltage relation to these voltages so,  should I consider using pullup on 3.6V rail on I2C and GPO lines safe and independent of the VCC? 

Magvel_0-1763967492762.png

 

JL. Lebon
JL. LebonBest answer
ST Employee
November 24, 2025

Hello, 

The voltage put on pull-up resistors on the I2C pins and on the GPO pin can be different than the voltage on the VCC pin (I2C and GPO are true open drain pins). This is off course if you are using the open drain version of the GPO pin (ST25DV04K-IE, not -JF version).

The maximum voltage indicated in the maximum rating table in the datasheet (-0.5 to 6.5V) indicates the max that you can reach before damaging the device. Nevertheless, it is not recommended to operate the device at 6.5V.

The recommended operating values are described in the "I2C operating conditions" table and specifies that the voltage should be between 1.8 and 5.5V.

So, you can have a VCC of 3.3V and have pull-ups resistors on GPO and SCL/SDA between 3.3V and 5.5V (you can't go below VCC since the VIH min is 0.75xVCC).

Best regards.

MagvelAuthor
Associate II
November 28, 2025

Can the same logic be valid for the MCU(STM32U083) running on 2.5v connected to ST25DV04 via I2C, with pullup to 3.6v?

JL. Lebon
ST Employee
December 1, 2025

Hello, 

Can you please ask this last question on the STM32 forum? It is the right place to get your answer.

Best regards.