Hi Nick,
Communications can be achieved in different modes and between devices in different roles.
Please find bellow the possible configurations:
- Passive mode
- RW (Reader <-> Card / Device Performing CE mode - CE/P2P Target)
- ST25R3911B
- ST25R3916
- ST25R395
- CE (CE <-> Reader/ Device in Poller mode - RW/P2P Initiator)
- Active Mode
In short, if you are looking to:
- communicate with cards or other devices in CE mode all devices can perform
- communicate with other devices in RW/P2P Initiator mode you can use ST25R3916
- communicate with the same device (ST25R <-> ST25R)
- In Active mode both ST25R3911B and ST25R3916 support AP2P
- In Passive mode the following configuration is possible: ST25R3916 <-> ST25R3916 and ST25R3911B (RW) <-> ST25R3916 (CE)
Please refer to the following links for additional information:
Best regards
GP