Hi,
Do you use a X-NUCLEO-NFC06A1 board (and X-CUBE-NFC6 Firmware) or a ST25R3916-DISCO board (and STSW-ST25R010 PC software) or a custom board (and ST RFAL firmware)?
ISO14443-3 does not define any tag memory organization. Different kinds of tags are relying on ISO14443-3 :
- T1 tags
- T2 tags
- T4 tags
- proprietary tags
If you are using the ST RFAL,
- see rfal_t1.c for T1 tag read/write API
- see rfal_t2.c for T2 tag read/write API
- see rfal_t4.c for T4 tag helpers API
Feel free to share more details about your tag (manufacturer an model).
Rgds
BT
In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.