Skip to main content
FDi R.14
Associate II
April 10, 2019
Solved

I can't found the implementation of rfalNfvPollerSelect and rfalNfvPollerReadSingleBlock

Hi, i have donwload the STM32CubeExpansion_NFC5_V1.3.0 but in the RFAL implementation there aren't the function rfalNfvPollerSelect and rfalNfvPollerReadSingleBlock (rfal_nfcv.c), i tried to use the old version ( rfalNfvSelect and rfalNfvReadSingleBlock) but dosn't work.

I read this old post:

https://community.st.com/s/question/0D50X00009XkWNXSA3/st25r3911b-calls-to-readwrite-block-after-successful-inventoryget-id

but there isn't any link to the new version of the library.

Can anyone give me the updated library link or can share thediff/patch ?

Where can I find STEVAL-SMARTAG1 reading examples with the X-NUCLEO-NFC05A1?

Thanks

Francesco

    This topic has been closed for replies.
    Grégoire Poulain
    ST Employee
    April 30, 2019

    Hi Francesco,

    The STEVAL-SMARTAG1 demo is composed by a ST25DV64K which supports the Fast Read Multiple Blocks.

    Therefore, yes you can exchange this command with a X-NUCLEO-NFC05A1 (ST25R3911B) on the STEVAL-SMARTAG1.

    Best regards

    GP

    3 replies

    Grégoire Poulain
    ST Employee
    April 25, 2019

    Hi Francesco,

    As you have well highlighted on the referred ticket, there was a typo and the APIs have been renamed.

    On more recent versions of the RFAL the APIs have been renamed as below:

    • rfalNfvPollerSelect -> rfalNfcvPollerSelect
    • rfalNfvPollerReadSingleBlock -> rfalNfcvPollerReadSingleBlock
    • ...

    The latest version of the ST25R3911B RFAL available is currently on the DISCO demo, here.

    Best regards

    GP

    FDi R.14
    FDi R.14Author
    Associate II
    April 29, 2019

    Oh thanks,

    i donwnload the last version and i found the function  iso15693FastReadMultipleBlocks(); does it work using it with  STEVAL-SMARTAG1 and X-NUCLEO-NFC05A1?

    Grégoire Poulain
    ST Employee
    April 30, 2019

    Hi Francesco,

    The STEVAL-SMARTAG1 demo is composed by a ST25DV64K which supports the Fast Read Multiple Blocks.

    Therefore, yes you can exchange this command with a X-NUCLEO-NFC05A1 (ST25R3911B) on the STEVAL-SMARTAG1.

    Best regards

    GP