Skip to main content
Associate III
January 11, 2025
Solved

How to test ST25DV NFC FTM mode transaction with MCU integration

 

Hi everyone,

I am currently working on a project involving the ST25DV NFC tag connected to a microcontroller (STM32). My goal is to test the Fast Transfer Mode (FTM) functionality. Here's the workflow I am aiming to achieve:

1. An NFC device (e.g., a smartphone) sends an FTM response/request to the ST25DV tag.

2. The microcontroller receives the FTM request/response from the ST25DV NFC tag and handles it accordingly.

I am looking for guidance on the following:

How can I simulate and verify the full FTM communication flow (NFC device ↔ ST25DV ↔ MCU)?

Are there any specific tools or software recommendations for testing FTM functionality?

Can I use ST25 NFC app to test FTM? Understand there is a app to test FTM demo using ST25 discovery kits. However I just need to test the transaction like send request to MCU thought FTM.

Regards,

This topic has been closed for replies.
Brian TIDAL
Brian TIDALBest answer
ST Technical Moderator
August 5, 2025

Hi,

When using the ST25 Android™ NFC Tap application, after tapping a tag, use the hamburger button to access the Send Custom Command option. You can then send raw commands.

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

3 replies

ST Employee
July 25, 2025

Below is a detailed guide to help you simulate, verify, and test the full FTM communication flow:


1. Understanding the FTM Communication Flow

  • NFC Device (e.g., smartphone) sends an FTM request to the ST25DV tag.
  • The ST25DV tag forwards this request to the MCU via its I2C/SPI interface.
  • The MCU processes the request and sends back a response to the ST25DV.
  • The ST25DV then transmits the response back to the NFC device.

2. Simulating and Verifying Full FTM Communication Flow

Hardware Setup

  • ST25DV NFC tag connected to your STM32 MCU via I2C or SPI.
  • NFC device (smartphone or NFC reader) to interact wirelessly with the ST25DV.

Steps to Verify FTM Flow

  1. Enable FTM on ST25DV:

    • Configure the ST25DV registers to enable Fast Transfer Mode.
    • Refer to the ST25DV datasheet and AN4247 application note for detailed register settings.
  2. MCU Firmware:

    • Implement an interrupt or polling mechanism to detect FTM requests from ST25DV.
    • Parse the incoming FTM request data.
    • Prepare and send the appropriate FTM response back to ST25DV.
  3. NFC Device Interaction:

    • Use an NFC device to send FTM requests.
    • Monitor the MCU logs/debug output to verify the request reception and response transmission.
  4. Debugging:

    • Use logic analyzers or I2C/SPI sniffers to monitor communication between ST25DV and MCU.
    • Use UART or SWO debug output on STM32 to trace firmware behavior.

3. Tools and Software Recommendations for Testing FTM

Tool/Software Purpose Notes

**ST25 NFC Application**NFC tag management and demo testingSTMicroelectronics app supports ST25DV and includes FTM demo for discovery kits.
**NFC-enabled Smartphone**To send custom FTM requestsUse NFC apps that allow raw NFC command sending.
**ST25DV Discovery Kit**Hardware platform with ST25DV and MCUUseful for reference firmware and FTM demo implementation.
**STM32CubeIDE + ST25DV Middleware**Develop and debug MCU firmwareST provides middleware libraries for ST25DV to ease integration.
**Logic Analyzer (e.g., Saleae)**Monitor I2C/SPI communication between ST25DV and MCUHelps verify timing and data correctness on the bus.

4. Using ST25 NFC App for FTM Testing

  • The ST25 NFC app by STMicroelectronics is primarily designed for:
    • Reading/writing NFC tags.
    • Demonstrating FTM on ST25 Discovery kits.
  • It can be used to send FTM requests to the ST25DV tag.
  • However, the app’s FTM demo is tailored for the Discovery kit environment.
  • For your use case (just sending FTM requests to MCU via ST25DV), you can:
    • Use the app to send FTM commands.
    • Monitor MCU response handling.
  • If you need more control over the FTM payload, consider:
    • Developing a custom NFC app (Android/iOS) that sends raw FTM commands.
    • Using NFC tools that allow sending custom NDEF or raw commands.

5. Additional Tips

  • Refer to ST25DV AN4247 Application Note: It contains detailed info on FTM operation and examples.
  • Firmware Examples: Check ST’s firmware packages for ST25DV and STM32 for FTM examples.
  • NFC Forum Compliance: Ensure your FTM commands comply with NFC Forum Type 5 Tag specs.
  • Debugging: Use serial output on STM32 to log received FTM requests and sent responses for easier troubleshooting.
chai2145Author
Associate III
July 26, 2025

Hi,

Thank you.

Use NFC apps that allow raw NFC command sending -> Can use the ST25 apps? I cannot find any tab to send raw NFC command.

 

regard,

kim

Brian TIDAL
Brian TIDALBest answer
ST Technical Moderator
August 5, 2025

Hi,

When using the ST25 Android™ NFC Tap application, after tapping a tag, use the hamburger button to access the Send Custom Command option. You can then send raw commands.

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.