Skip to main content
muthu kural
Visitor II
September 21, 2017
Solved

How to Read/Write ST25TA02K-PC6H5 NFC

Posted on September 21, 2017 at 16:40

Hello,

I am working on Project which have ST25TA02K-PC6H5 as a portion. I am seeing that interface between MCU and the NFC is the GPIO pin only.Neither have I2C nor SPI.  With the GPIO pin, How can I read/write the NFC registers? 

0690X00000608JoQAI.png

Have I selected wrong part?

Please suggest.

Thanks,

Muthu

    This topic has been closed for replies.
    Thomas Q.
    Thomas Q.Best answer
    ST Employee
    September 22, 2017
    Posted on September 22, 2017 at 14:54

    Hello,

    The GPO pin of the ST25TA02K-P is an output-only signal used to trigger RF events

    (see section 2.4 and section 11 of the

    http://www.st.com/content/ccc/resource/technical/document/datasheet/f9/9f/ef/57/ef/20/48/d0/DM00179249.pdf/files/DM00179249.pdf/jcr:content/translations/en.DM00179249.pdf

    ).

    In the diagram you are showing, a typical use-case would be to send a wakeup signal

    from the ST25TA02K-P to the microcontroller on a user-defined RF event.

    The GPO interface can not be used to transmit NDEF content.

    I suggest you have a look at the

    http://www.st.com/en/nfc/m24sr-series-dynamic-nfc-tags.html?querycriteria=productId=SS1812

     product, which is a NFC Type 4A tag providing

    a I2C interface that can be used to access the EEPROM.

    Best regards

    1 reply

    Thomas Q.
    Thomas Q.Best answer
    ST Employee
    September 22, 2017
    Posted on September 22, 2017 at 14:54

    Hello,

    The GPO pin of the ST25TA02K-P is an output-only signal used to trigger RF events

    (see section 2.4 and section 11 of the

    http://www.st.com/content/ccc/resource/technical/document/datasheet/f9/9f/ef/57/ef/20/48/d0/DM00179249.pdf/files/DM00179249.pdf/jcr:content/translations/en.DM00179249.pdf

    ).

    In the diagram you are showing, a typical use-case would be to send a wakeup signal

    from the ST25TA02K-P to the microcontroller on a user-defined RF event.

    The GPO interface can not be used to transmit NDEF content.

    I suggest you have a look at the

    http://www.st.com/en/nfc/m24sr-series-dynamic-nfc-tags.html?querycriteria=productId=SS1812

     product, which is a NFC Type 4A tag providing

    a I2C interface that can be used to access the EEPROM.

    Best regards