Skip to main content
Sandhu
Associate
July 26, 2021
Solved

How to configure External power amplifier gain? Internal power amplifier is able to control using txRxCfg.txOutputLevel. How to configure external power amplifier?

..

This topic has been closed for replies.
Nick K
Nick KBest answer
ST Employee
August 3, 2021

Its done the same way. The register to adjust the output level works on the output of the external or internal PA.

When using an external PA the amplifier source is changed but the RF output signal is still controlled with the register ST25RU3993_REG_MODULATORCONTROL3 via the bits Tx_lev[0..2] and Tx_lev[3..4]

BR

Nick

1 reply

Nick K
Nick KBest answer
ST Employee
August 3, 2021

Its done the same way. The register to adjust the output level works on the output of the external or internal PA.

When using an external PA the amplifier source is changed but the RF output signal is still controlled with the register ST25RU3993_REG_MODULATORCONTROL3 via the bits Tx_lev[0..2] and Tx_lev[3..4]

BR

Nick