Skip to main content
MLust.1
Visitor II
March 27, 2020
Solved

Hi, I'm intrestid in developing using st25ru3993 (without eval board) So, onestly, ST oficcial code example is... difficult for understanding in some cases. I'll I will be grateful if smd will give me some code example of read/write process Thank you

It's my first experience of web question, so I hope for your understanding

    This topic has been closed for replies.
    Cedric Dalban
    Cedric DalbanBest answer
    ST Employee
    March 30, 2020

    ​Hello MLust,

    Reading/Writing and more generally accessing a tag is really simple.

    The example code is provided in function demo_evalAPI_Gen2RdWr() from file STUHFL_demoEvalApi.c.

    Let me explain the code:

    •    printGen2InventoryInfo(&invData); 

    => lists all tags available in antenna range

    => invData contains the full list of all inventoried tags

    => the first entry (the first tag) will be used for reading/writing

    • gen2Select(invData.tagList[0].epc.data, invData.tagList[0].epc.len);

    => by default, the read/writes/all access will be done on first visible tag

    => the Gen2_Select() call creates filters to ensure all susequent read/writes will be done on same tag

    => as mentioned above the first entry is used for subsequent accesses thus the ceration of filter on tagList[0]

    • void gen2Read(uint8_t *data)

    => prepares readData parameters that follows Gen2 specifications

    • membank: bank from which data will be read
      • wordPtr: start pointer (in words) from which data will be read
      • bytes2read: number of bytes to read
      • pwd: access password (if any, by default must be set to 0x00000000)

    => launches data read:

    • data : contains data read from tag

    • void gen2Write(uint16_t data)

    => prepares writeData parameters that follows Gen2 specifications

    • membank: bank to which data will be written
      • wordPtr: start pointer (in words) to which data will be written
      • data: data to be written (can only write word per word)
      • pwd: access password (if any, by default must be set to 0x00000000)

    That's all you need to write/read data to/from tag,

    similar functions can be called to lock, kill, ... the tags.

    best regards,

    Cedric

    1 reply

    Cedric Dalban
    Cedric DalbanBest answer
    ST Employee
    March 30, 2020

    ​Hello MLust,

    Reading/Writing and more generally accessing a tag is really simple.

    The example code is provided in function demo_evalAPI_Gen2RdWr() from file STUHFL_demoEvalApi.c.

    Let me explain the code:

    •    printGen2InventoryInfo(&invData); 

    => lists all tags available in antenna range

    => invData contains the full list of all inventoried tags

    => the first entry (the first tag) will be used for reading/writing

    • gen2Select(invData.tagList[0].epc.data, invData.tagList[0].epc.len);

    => by default, the read/writes/all access will be done on first visible tag

    => the Gen2_Select() call creates filters to ensure all susequent read/writes will be done on same tag

    => as mentioned above the first entry is used for subsequent accesses thus the ceration of filter on tagList[0]

    • void gen2Read(uint8_t *data)

    => prepares readData parameters that follows Gen2 specifications

    • membank: bank from which data will be read
      • wordPtr: start pointer (in words) from which data will be read
      • bytes2read: number of bytes to read
      • pwd: access password (if any, by default must be set to 0x00000000)

    => launches data read:

    • data : contains data read from tag

    • void gen2Write(uint16_t data)

    => prepares writeData parameters that follows Gen2 specifications

    • membank: bank to which data will be written
      • wordPtr: start pointer (in words) to which data will be written
      • data: data to be written (can only write word per word)
      • pwd: access password (if any, by default must be set to 0x00000000)

    That's all you need to write/read data to/from tag,

    similar functions can be called to lock, kill, ... the tags.

    best regards,

    Cedric