Hi,
ST25R3911/12 etc are built for crystals of 13.56/27.12 MHZ and a carrier frequency of 13.56. There is the possibility to use an external clock like described here: https://community.st.com/s/question/0D53W00000CPX6qSAH/is-it-possible-to-use-a-clock-oscillator-instead-of-quartz-crystal-oscillator
However it is not built for running a carrier not equal to 13.56 MHz. And with a 19.2 MHz clock you would need to run the carrier at 8.6MHz (Runnig 19.2 MHz you will likely run into internal chip issues). Theoretically most of the time settings would shift as a result to the new fc. However that is probably not what you want to achieve:
You are falling out of ISM band and all existing infrastructure is only built/optimized/matched for 13.56 MHz.
Regards, Ulysses