Skip to main content
KKost.2
Visitor II
January 18, 2022
Solved

Handing the WTX frame correctly

Hello,

I would like to verify if my approach to handling the WTX S-block over I2C is correct.

Currently when I send "update binary" command with data field longer than 2 bytes I receive the S(WTX) frame in response, which is expected.

The command is:

x03 x00 xD6 x00 x3E x06 xF1 xF2 xF3 xF4 xF5 xF6 xB5 x81 (send)

The received frame is:

xF2 x02 x0A x72 (recv)

Immediately after receiving this frame I stop reading the I2C further, wait for 9.6*2 ms and send identical frame as a response:

wait(9.6*2 ms)

xF2 x02 x0A x72 (send)

Then I still attempt to read the R-APDU for "update binary" however nothing is received from the I2C.

The data gets properly written as the I am able to confirm with "read binary".

So, my question is - should I still expect the normal R-APDU for "update binary" if the WTX is received? I'm quite sure this is the case, just need a sanity check :)

Thanks,

Chris

This topic has been closed for replies.
Brian TIDAL
Brian TIDALBest answer
ST Technical Moderator
January 18, 2022

Hi Chris,

I guess your question is related to the M24SR. In that case, I would recommend to base application developments on top of X-CUBE-NFC1 package.

If I am not wrong, the R-APDU for Update Binary is sent as a response to the S(WTX) sent by the host. Can you try to remove the wait(9.6*2 ms) and to send the S(WTX) just after the received S(WTX) and then poll for I2C readiness with a timeout large enough (let say 200ms) and read the response?

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

1 reply

Brian TIDAL
Brian TIDALBest answer
ST Technical Moderator
January 18, 2022

Hi Chris,

I guess your question is related to the M24SR. In that case, I would recommend to base application developments on top of X-CUBE-NFC1 package.

If I am not wrong, the R-APDU for Update Binary is sent as a response to the S(WTX) sent by the host. Can you try to remove the wait(9.6*2 ms) and to send the S(WTX) just after the received S(WTX) and then poll for I2C readiness with a timeout large enough (let say 200ms) and read the response?

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.