Skip to main content
Associate II
October 17, 2025
Solved

Getting started with NFC081A

Hi. I bought a set of "NUCLEO-L476RG" and "NUCLEO-NFC08A1".
The "X-CUBE-NFC6" library for the "NUCLEO-L476RG" contains examples of "NFC08A1_PollingTagDetect" and "NFC08A1_PollingTagDetectNDEF."

How do I run them in the STM32 IDE?
Which one should I use to read the tags and output data via UART?

Please, could you help with that? I'm a beginner with NFC and all my attempts to run it - failed.
The instructions included with the library are uninformative.

This topic has been closed for replies.
Brian TIDAL
Brian TIDALBest answer
ST Technical Moderator
October 17, 2025

Hi,

just go to <yourHomeDir>\STM32Cube\Repository\Packs\STMicroelectronics\X-CUBE-NFC6\3.1.0\Projects\NUCLEO-L476RG\Applications\NFC08A1_PollingTagDetect\STM32CubeIDE, launch the .project or the .cproject in STM32CubeIDE

Build the project and flash it.

Open a terminal (e.g.TeraTerm) on the STMicroelectronics STLink Virtual Com Port at 115200.

This should work.

You can also directly download the pre-build binary available in <yourHomeDir>\\STM32Cube\Repository\Packs\STMicroelectronics\X-CUBE-NFC6\3.1.0\Projects\NUCLEO-L476RG\Applications\NFC08A1_PollingTagDetect\Binary with STM32CubeProgrammer

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

1 reply

Brian TIDAL
Brian TIDALBest answer
ST Technical Moderator
October 17, 2025

Hi,

just go to <yourHomeDir>\STM32Cube\Repository\Packs\STMicroelectronics\X-CUBE-NFC6\3.1.0\Projects\NUCLEO-L476RG\Applications\NFC08A1_PollingTagDetect\STM32CubeIDE, launch the .project or the .cproject in STM32CubeIDE

Build the project and flash it.

Open a terminal (e.g.TeraTerm) on the STMicroelectronics STLink Virtual Com Port at 115200.

This should work.

You can also directly download the pre-build binary available in <yourHomeDir>\\STM32Cube\Repository\Packs\STMicroelectronics\X-CUBE-NFC6\3.1.0\Projects\NUCLEO-L476RG\Applications\NFC08A1_PollingTagDetect\Binary with STM32CubeProgrammer

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.