Skip to main content
Joerg Maertens
Visitor II
January 4, 2017
Solved

generate CRC for M24SR

Posted on January 04, 2017 at 15:39

Hi everyone,

in our application I have to communicate with a M24SR02-Y over IIC.

I have tried 2 versions to generate the CRC:

Version 2

#define PRESET_VALUE 0x6363

#define MASK 0x8408

#define NUMBER_OF_BYTES 6

unsigned char array_of_databytes[6] = { 0x03, 0x00, 0xB0, 0x00, 0x00, 0x02 };

void CRC() {

    current_crc_value = PRESET_VALUE;

    for (i = 0; i < NUMBER_OF_BYTES; i++)    {

        DATA = array_of_databytes[i];

        current_crc_value ^= (uint)DATA;

        for (j = 0; j < 8; j++)  {

            if ((current_crc_value & 0x0001) > 0)  {

                current_crc_value >>= 1;

                current_crc_value ^= MASK;

            }

            else            {

                current_crc_value >>= 1;

            }

        }

}

Version 2

#define PRESET_VALUE 0x6363

#define NUMBER_OF_BYTES 6

unsigned char array_of_databytes[6] = { 0x03, 0x00, 0xB0, 0x00, 0x00, 0x02 };

void CRC() {

    current_crc_value = PRESET_VALUE;

    for (i = 0; i < NUMBER_OF_BYTES; i++)    {

        DATA = array_of_databytes[i];

        DATA ^= (uchar)(current_crc_value & 0x00FF);

        DATA ^= (DATA<<4);

        current_crc_value >>= 8;

        current_crc_value ^= (uint)DATA << 8;

        current_crc_value ^= (uint)DATA << 3;

        current_crc_value ^= (uint)DATA >> 4;

    }

}

Version 2 based on AN4420 page 20.

Both version generate a CRC 0x7940.

But according to AN4433 'Storing data into the NDEF memory of M24SR' on page 20 the CRC has to be 0x7D6B.

The databyte array

{ 0x03, 0x00, 0xB0, 0x00, 0x00, 0x02 }

contains PCB and command of the 'Read NDEF message length' command.

What could have gone wrong?

Thanks,

Jörg

This topic has been closed for replies.
Berenice BENVEGUDA
ST Technical Moderator
January 20, 2017
Posted on January 20, 2017 at 16:48

Dear Joerg,

You're right the correct CRC is 0x7940. There is a mistake in AN4433.

This will be corrected soon.

Thanks a lot for your help !

Best Regards,

NFC Product Support1

1 reply

Berenice BENVEGUDA
ST Technical Moderator
January 20, 2017
Posted on January 20, 2017 at 16:48

Dear Joerg,

You're right the correct CRC is 0x7940. There is a mistake in AN4433.

This will be corrected soon.

Thanks a lot for your help !

Best Regards,

NFC Product Support1