Skip to main content
Brad Goodman
Associate
January 11, 2023
Solved

Fundamental ST25DV64 Register Write problems

Am in the infancy of a proof-of-concept investigation with ST25DV64. I have been able to do some read/writes with NFC without issue - and am working on the i2c side.

We are working with a custom/proprietary system/i2c stack so I don't have much off-the-shelf code to fall back on, but I've written what seems to be a proper implementation of the basic register read/write protocols outlined in ST25DV64 datasheet - and they MOSTLY work.

I can read the NFC NDEF data via i2c from registers at i2c address 0x53, device addresses 0 - 32.I am also getting what appears to be valid Dynamic Configuration registers via device 0x53 register addresses 0x2000-2007 as such:

2000: 88 ff 08 00 00 00 00 00

Which seem to be a valid representation of the initial state of these registers. I can also write and modify one of the GPO bits and read it back

But here's where things get weird:

If I write like an 0x08 to location 2000 - it seems to turn off the high 8 bit. But If I write a 0xff I read back an 0x88. If I write a 0x00 - I always get a 0x08. In other words - I only seem to have control of the high bit in this register.

Write to 0x2002 or 0x2003 will get acked back - but 0x2006 does not.

I can verify with the i2c decoder on my scope that at least the scope believes the signals are good, and I have bumped the I2C speed up and down orders of magnitude (and although at some levesls this stops working) - this specific behavior of these registers remain unchanged.

From what I can tell - these are the first registers that I should be writing to enable other functionality in other registers.

Is there a signaling problem here, or an I doing something complete wrong?

This topic has been closed for replies.
JL. Lebon
JL. LebonBest answer
ST Employee
January 26, 2023

If you are using the mailbox to transfer data between RF and I2C, you don't need a synchro block as it is already present in the form of the MB_CRTL_Dyn register.

If you are using the EEPROM to exchange data, then you can use a synchro block. You may then use an EEPROM memory block (but be careful on cycling on this block), or as you suggest, you can write a "synchro message" in the mailbox. But using EEPROM and mailbox at the same time is constraining: when FTM is enabled (MB_CTRL_Dyn[MB_EN]=1), it is not possible to write into EEPROM. So you would need to enable FTM when writing synch message and disabling it again when you want to write into EEPROM.

Best regards.

15 replies

Brad Goodman
Associate
January 26, 2023

Thanks - that makes sense.

Are you implying the "synchro block" should be in eeprom and not a mailbox? (Due to the mailbox being singular, in that you have to write your whole message out from zero each time?) Or could my "syncro block" be the first x bytes of the mailbox?

JL. Lebon
JL. LebonBest answer
ST Employee
January 26, 2023

If you are using the mailbox to transfer data between RF and I2C, you don't need a synchro block as it is already present in the form of the MB_CRTL_Dyn register.

If you are using the EEPROM to exchange data, then you can use a synchro block. You may then use an EEPROM memory block (but be careful on cycling on this block), or as you suggest, you can write a "synchro message" in the mailbox. But using EEPROM and mailbox at the same time is constraining: when FTM is enabled (MB_CTRL_Dyn[MB_EN]=1), it is not possible to write into EEPROM. So you would need to enable FTM when writing synch message and disabling it again when you want to write into EEPROM.

Best regards.

Brad Goodman
Associate
January 26, 2023

Are you saying that my RF (phone) should be polling MB_CTRL_Dyn, directly, to see if there is an i2c-generated message awaiting receipt?

JL. Lebon
ST Employee
January 26, 2023

If you are doing transfer via the mailbox (i.e. your I2C controller is writing messages into the mailbox), then yes, the right procedure for the RF reader is to read (polling) the MB_CTRL_Dyn register to know if there is a message from I2C available in the mailbox.