Skip to main content
esoft.1
Visitor II
April 18, 2023
Question

External PA not working.

Dear sir

It is being developed on the ST25ru3993 board. The external PA is not working, so I checked the power and it is 0V. The documentation says it should be 4.1V, but I want to know if I can make it work again.

Also, I want to know why the expansion PA is not powered.

​

If I configure another external PA circuit and use it, I wonder if I can operate it with that board.

​

If this is possible, I would like a circuit recommendation.

​

Thank you, sir

This topic has been closed for replies.

1 reply

Marcel Rossignol
ST Employee
June 12, 2023

Dear esoft.1,

please could describe, which software are you using?

Is it an own software or do you use the ST software for controlling the board?

Thanks & best regards,

Marcel