Error 87 issue while reading tag using CR95HF-VMD5T NFC transceiver chip.
- 10 replies
- 3091 views
Hi,
We have developed a NFC reader design using the CR95HF-VMD5T chip. Our design is similar to the X-NUCLEO-NFC03A1 development board, its just we have used a flex NFC antenna by PulseLarsen with part number W7001.
The issue we are facing is that the board is unable to read a tag and returns error 87, with the firmware we have written.
We have tested our firmware on the X-NUCLEO-NFC03A1 development board and we are able to read a tag without any problem.
We also probed the antenna pads of both our board and X-NUCLEO-NFC03A1 using an oscilloscope just to see if we see any difference in the signal. What we noticed was that the X-NUCLEO-NFC03A1 board was showing a 10V peak-to-peak sine wave at 13.5Mhz whereas our board was showing around 3.4V peak-to-peak around the same frequency.
We wanted to know if this is the reason for our problem and a solution for that or if something else is going on that we're missing.
I have attached the antenna's datasheet for reference.
Thanks
Brosnan Gomes
Hardware Developer Engineer
+917972046516
Mrinq Technologies