Skip to main content
Associate II
January 17, 2025
Solved

Does ST25DV64KC (X-NUCLEO-NFC07A1) Nucleo Expansion board work with Arduno Uno ?

Hi,

Can anybody tell me whether the X-NUCLEO-NFC07A1 works with an Arduno Uno ?

In other words, can I just plug an Arduno Uno onto this unit, or do I need to buy a STM32 development board ?

When plugging it onto a normal Arduno Uno I am unable to read an NFC tag (13.56 Mhz).

Please help.

Thanks

This topic has been closed for replies.
Brian TIDAL
Brian TIDALBest answer
ST Technical Moderator
January 17, 2025

Hi,

Check that the jumper on the X-NUCLEO-NFC07A1 ST1 connector is in place. This jumper provides the required voltage to the device on the board. See UM2960 Getting started with the X-NUCLEO-NFC07A1 NFC/RFID tag IC expansion board based on ST25DV64KC for STM32 Nucleo §1.2 Board setup.

Also, the IOREF might need to be disconnected if 5V is provided by the arduino board on this pin as CN6.2 (IOREF) and CN6.4 (3V3) are connected together in the X-NUCLEO-NFC07A1. You can just bend th CN6.2 pin on the X-NUCLEO-NFC07A1.

"When plugging it onto a normal Arduno Uno I am unable to read an NFC tag (13.56 Mhz)." do you mean not able to communicate through I2C or not able to communicate through RF?

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

1 reply

Brian TIDAL
Brian TIDALBest answer
ST Technical Moderator
January 17, 2025

Hi,

Check that the jumper on the X-NUCLEO-NFC07A1 ST1 connector is in place. This jumper provides the required voltage to the device on the board. See UM2960 Getting started with the X-NUCLEO-NFC07A1 NFC/RFID tag IC expansion board based on ST25DV64KC for STM32 Nucleo §1.2 Board setup.

Also, the IOREF might need to be disconnected if 5V is provided by the arduino board on this pin as CN6.2 (IOREF) and CN6.4 (3V3) are connected together in the X-NUCLEO-NFC07A1. You can just bend th CN6.2 pin on the X-NUCLEO-NFC07A1.

"When plugging it onto a normal Arduno Uno I am unable to read an NFC tag (13.56 Mhz)." do you mean not able to communicate through I2C or not able to communicate through RF?

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.