Skip to main content
CLemb.1
Visitor II
October 4, 2020
Solved

Dear all, we are using the ST25DV04K_IER6C3 EEPROM with energy harvesting, however from the begiining the EH is deactivated and has to be activiated with the PC Software -is there a possibilty that the EH mode is allwoed from beginning? Thanks Christ

..

    This topic has been closed for replies.
    JL. Lebon
    JL. LebonBest answer
    ST Employee
    October 5, 2020

    ​Hello,

    There is two ways of activating energy harvesting:

    • dynamically enable/disable energy harvesting, using the dynamic register EH_CTRL_Dyn
    • enable/disable energy harvesting at boot, using the static configuration register EH_MODE

    In your case, if you want to enable energy harvesting at boot (energy harvesting will be delivered as soon as the field power is strong enough), you need to write 0 in the EH_MODE static register. This can be done by RF or I2C. You first need to open the corresponding security session by presenting the right password (RF password 0 or I2C), then from RF, send a Write Configuration command at address 02h with value 1, or by I2C, write 01 at address 2002h. The EH_MODE static register is non volatile.

    Best regards.

    1 reply

    JL. Lebon
    JL. LebonBest answer
    ST Employee
    October 5, 2020

    ​Hello,

    There is two ways of activating energy harvesting:

    • dynamically enable/disable energy harvesting, using the dynamic register EH_CTRL_Dyn
    • enable/disable energy harvesting at boot, using the static configuration register EH_MODE

    In your case, if you want to enable energy harvesting at boot (energy harvesting will be delivered as soon as the field power is strong enough), you need to write 0 in the EH_MODE static register. This can be done by RF or I2C. You first need to open the corresponding security session by presenting the right password (RF password 0 or I2C), then from RF, send a Write Configuration command at address 02h with value 1, or by I2C, write 01 at address 2002h. The EH_MODE static register is non volatile.

    Best regards.