Skip to main content
AWate.1
Associate
April 25, 2022
Solved

CSharp_Dll3911_Demo won't compile

I'm looking at the Dll3911_Demos from Discovery GUI pack v1.2.12.

Frustratingly it It wont compile due to an error on line 202

ErrorCode = ST25R3911_Dll.rfalTransceiveBlockingTxRx(Handle, cmd, 5, resp, 12, us, RFAL, rfalConvMsTo1fc(5));

The function rfalConvMsTo1fc seems to be missing also the variable RFAL. I can compile it if i comment out the line but this is function I would like to implement.

Is there a more up to date version of the source code which compiles available?

This topic has been closed for replies.
Ulysses HERNIOSUS
ST Technical Moderator
April 26, 2022

Hi,

Demo_IsoDep.cpp contains the sequences you are wishing for. Unfortunately that demo is not ported to C# but it should give you a straightforward way to achieve the same in C#.

Best Regards, Ulysses

5 replies

Ulysses HERNIOSUS
ST Technical Moderator
April 26, 2022

Hi,

I was looking at the demo and for me it compiles without issues. I was also not able to locate such a line as mentioned by you.

Could you describe in more detail what your are doing and the exact error message?

BR, Ulysses.

AWate.1
AWate.1Author
Associate
April 26, 2022

Hi,

Appologies I just redownloaded the package and did a fresh install and your correct the line isn't there.

I'm trying to call the ISO-DEP command that you demonstrate in your GUI to send through custom APDU's to the ticket once a connection has been established.

0693W00000Lz0x5QAB.pngI assume i tried to do this previously but was unsure what to set for the parameters uint flags, uint fwt

Thanks in advance for any help you can provide in this manner.

Ulysses HERNIOSUS
ST Technical Moderator
April 26, 2022

Hi,

Demo_IsoDep.cpp contains the sequences you are wishing for. Unfortunately that demo is not ported to C# but it should give you a straightforward way to achieve the same in C#.

Best Regards, Ulysses

AWate.1
AWate.1Author
Associate
April 26, 2022

Thats perfect, thanks for your help!!!

ST Employee
April 26, 2022

the rfalConvMsTo1fc is just a macro that multiply the parameter by 13560

#define rfalConvMsTo1fc( t )  ( (t) * 13560 )    /*!< Converts the given t from ms to 1/fc    */

So just change rfalConvMsTo1fc(5) by (5 * 13560).

The 'RFAL' variable corresponds to the flags parameter of rfalTransceiveBlockingTxRx. So put the right value and it should work