Hi Michael,
the antenna on the PLUG-CR95HF-B board has the following characteristics:
- dimension: 43 x 34 mm.
- number of turns: 2
the antenna on the X-NUCLEO-NFC03A1 board has the following characteristics:
- dimension: 47 x 34mm
- number of turns: 4
I will try to grab a PLUG-CR95HF-B and make some read range tests and detection range tests. On your side, can you request your local distributor to send you an X-NUCLEO-NFC03A1 board?
For your own design, ST provides the following application note and calculation tool that should help to improve the performances
- AN5248: ST25R95 transceiver antenna tuning circuit with EMI filter
- STSW-ST25R003: antenna tuning circuit with EMI filter calculation tool
Also, feel free to send to me (in private) your schematics so that I can manage to have them being reviewed by RF experts team.
Note: if you change the antenna on the PLUG-CR95HF-B, the matching circuit will need to be updated.
I would also recommend to base your firmware on top of ST RF Abstraction Layer (RFAL) firmware provided in X-CUBE-NFC3 v2.0.0: this RFAL abstracts the reader being used so that you can easily move to ST25R3911B or ST25R3916 reader in case high performances are needed without having to change your code. The RFAL can be easily tailored to fit your flash/ram constraints.
Regarding the calibration, make sure to calibrate when no tag are in in the operating volume. Make sure to have no metallic parts (cables, ...) under the antenna. With my X-NUCLEO-NFC03A1, in Idle mode, I am able to detect a Type 4A tag at ~3 cm and then able to read it.
Rgds
BT
In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.