Skip to main content
Siddhesh Nadkarni
Visitor II
May 1, 2018
Solved

CR95HF responding with 0x8300

Posted on May 01, 2018 at 22:37

Hi,

We are working with the CR95HF chip using SPI protocol.

We get the correct response for echo, protocol set (1443-A) and IDn.

However for a continuous SendAndRecv command with the value 0x04022607 we get the response 0x8300 which is unknown instead of 0x8700 since there is no tag in the field.

Any recommendations with this issue ?

Regards,

Sid
    This topic has been closed for replies.
    Peter Boringer
    Peter BoringerBest answer
    Visitor II
    May 31, 2018
    Posted on May 31, 2018 at 14:30

    Hello Siddhesh,

    The error code 0x8300 provided by the CR95HF is relative to a bad protocol select command. You might check with a tag ISO 14443 A in front of the reader that you can access it with the send/receive command. I believe that their is a mismatch in your protocol select command and so you got the error code associated to this bad command setting.

    Best regards

    PB

    1 reply

    Peter Boringer
    Peter BoringerBest answer
    Visitor II
    May 31, 2018
    Posted on May 31, 2018 at 14:30

    Hello Siddhesh,

    The error code 0x8300 provided by the CR95HF is relative to a bad protocol select command. You might check with a tag ISO 14443 A in front of the reader that you can access it with the send/receive command. I believe that their is a mismatch in your protocol select command and so you got the error code associated to this bad command setting.

    Best regards

    PB