Skip to main content
RSing.9
Associate
August 27, 2021
Solved

CR95HF not coming in ready state.

..

    This topic has been closed for replies.
    Brian TIDAL
    Brian TIDALBest answer
    ST Technical Moderator
    August 27, 2021

    Hi,

    can you share more details about your hardware setup:

    • do you use your own custom board or do you use existing board (such as X-NUCLEO-NFC03A1 connected to an MCU board)
    • how is connected the CH95HF to the MCU: PCB connection or wire jumpers? If wire jumpers are used, verify them
    • what is the setup of the SSI_0 and SSI_1 pins? Can you probe those 2 signals during startup and make sure SSI_0=1 and SSI_1=0
    • can you check that the CR95HF is properly powered

    Regarding the startup sequence, before sending the ECHO sequence, can you send a poll command and check that bit 2 is set in the poll answer?

    Rgds

    BT

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

    4 replies

    RSing.9
    RSing.9Author
    Associate
    August 27, 2021
    RSing.9
    RSing.9Author
    Associate
    August 27, 2021

    I am using nrf52832 with CR95HF

    here are basic functions for CR95HF

    void reset_cr95hr(unsigned int ch)
    {
     nrf_gpio_pin_clear(SPI_CS[ch]);
     nrf_delay_ms(1);
     SPI_byte_send(0x01);
     nrf_gpio_pin_set(SPI_CS[ch]);
     nrf_delay_ms(100);
    }
     
     
    char EchoResponse(unsigned int ch) {
     int ii=5, tmp;
     nrf_gpio_pin_clear(SPI_CS[ch]);
     nrf_delay_ms(1);
     SPI_byte_send(0x00); // Send cmd to CR95HF
     SPI_byte_send(ECHO);
     nrf_gpio_pin_set(SPI_CS[ch]);
     
     while(1){
     
     nrf_gpio_pin_clear(SPI_CS[ch]);
     nrf_delay_ms(1);
     SPI_byte_send(0x03);
     tmp = SPI_byte_receive();
     nrf_gpio_pin_set(SPI_CS[ch]);
     
     if((tmp & 0x08) >> 3){
     nrf_gpio_pin_clear(SPI_CS[ch]);
     nrf_delay_ms(1);
     SPI_byte_send(0x02);
     tmp = SPI_byte_receive();
     nrf_gpio_pin_set(SPI_CS[ch]);
     if(tmp == ECHO){
     return 1;
     }
     return 0;
     }
     }
    }
     
    void writeCmd(unsigned short cmd, unsigned short dataLen, unsigned int ch){
     unsigned short i = 0;
     
     nrf_gpio_pin_clear(SPI_CS[ch]);
     nrf_delay_ms(1);
     SPI_byte_send(0x00); // Send cmd to CR95HF
     SPI_byte_send(cmd);
     SPI_byte_send(dataLen);
     while (dataLen == 0){
     nrf_gpio_pin_set(SPI_CS[ch]);
     break;
     }
     for(i=0; i<dataLen; i++){
     SPI_byte_send(sdata[i]);
     }
     nrf_gpio_pin_set(SPI_CS[ch]);
    }
     
    void readCmd(unsigned int ch){
     unsigned short i = 0, ii=2;
     
     while(ii){
     ii--;
     nrf_gpio_pin_clear(SPI_CS[ch]);
     nrf_delay_ms(1);
     SPI_byte_send(0x03);
     res = SPI_byte_receive();
     nrf_gpio_pin_set(SPI_CS[ch]);
     
     if((res & 0x08) >> 3){
     nrf_gpio_pin_clear(SPI_CS[ch]);
     nrf_delay_ms(1);
     SPI_byte_send(0x02);
     res = SPI_byte_receive();
     dataNum = SPI_byte_receive();
     for(i=0; i<dataNum; i++)
     rdata[i] = SPI_byte_receive();
     nrf_gpio_pin_set(SPI_CS[ch]);
     break;
     }
     nrf_gpio_pin_set(SPI_CS[ch]);
     nrf_delay_ms(1);
     }
    }
     
    void IndexMod_Gain(unsigned int ch) {
     sdata[0] = 0x09;
     sdata[1] = 0x04;
     sdata[2] = 0x68;
     sdata[3] = 0x01;
     sdata[4] = 0x01;
     sdata[5] = 0x50;
     writeCmd(WrReg, 6, ch);
     readCmd(ch);
    }
     
    void AutoFDet(unsigned int ch)
    {
     sdata[0] = 0x09;
     sdata[1] = 0x04;
     sdata[2] = 0x0A;
     sdata[3] = 0x01;
     sdata[4] = 0x02;
     sdata[5] = 0xA1;
     writeCmd(WrReg, 6,ch);
     readCmd(ch);
    }
     
    void Select_ISO_IEC_14443_A_Protocol(unsigned int ch) {
     sdata[0] = 0x02;
     sdata[1] = 0x00;
     writeCmd(ProtocolSelect, 2, ch);
     readCmd(ch);
     
     // Clear read and write buffers
     for(j=0; j<18; j++ ){
     rdata[j] = 0;
     sdata[j] = 0;
     }
    }
     
    void Select_ISO_IEC_18092_Protocol(unsigned int ch) {
     sdata[0] = 0x04;
     sdata[1] = 0x51;
     writeCmd(ProtocolSelect, 2, ch);
     readCmd(ch);
     
     // Clear read and write buffers
     for(j=0; j<18; j++ ){
     rdata[j] = 0;
     sdata[j] = 0;
     }
    }
     
     
    void GetNFCTag(unsigned int ch) {
     sdata[0] = 0x00;
     sdata[1] = 0xFF;
     sdata[2] = 0xFF;
     sdata[3] = 0x00;
     sdata[4] = 0x00;
     writeCmd(SendRecv, 5, ch);
     readCmd(ch);
     
     if(res & 0x80){
     for(j=0; j<dataNum; j++){
     ByteToHex(rdata[j], txt_hex);
     strcat(ID, txt_hex);
     }
     NFC_Flag = 1; 
     }
     else {
     NFC_Flag = 0; 
     Select_ISO_IEC_14443_A_Protocol(ch);
     }
    }
     
    void ByteToHex(char input, char *output)
    {
     unsigned int ii,jj;
     
     
     ii=(input>>4)&0x0f;
     if(ii<10)
     {
     ii+=0x30;
     }
     else
     {
     ii+=55;
     }
     jj=input&0x0f;
     if(jj<10)
     {
     jj+=0x30;
     }
     else
     {
     jj+=55;
     }
     
     txt_hex[0]=ii;
     txt_hex[1]=jj;
     txt_hex[2]=0;
    }
     
     
    void GetTagID(unsigned int ch) {
     sdata[0] = 0x26;
     sdata[1] = 0x07;
     writeCmd(SendRecv , 2, ch);
     readCmd(ch);
     
     sdata[0] = 0x93;
     sdata[1] = 0x20;
     sdata[2] = 0x08;
     writeCmd(SendRecv , 3, ch);
     readCmd(ch);
     
     if(res & 0x80) {
     for(j=1; j<dataNum-3; j++) {
     ByteToHex(rdata[j], txt_hex);
     strcat(ID, txt_hex);
     }
     TAG_Flag = 1; 
     }
     else {
     TAG_Flag = 0; 
     Select_ISO_IEC_14443_A_Protocol(ch);
     }
    }
     
    void Calibration(unsigned int ch)
    {
     // Calibrate CR95HF device
     sdata[0] = 0x03;
     sdata[1] = 0xA1;
     sdata[2] = 0x00;
     sdata[3] = 0xF8;
     sdata[4] = 0x01;
     sdata[5] = 0x18;
     sdata[6] = 0x00;
     sdata[7] = 0x20;
     sdata[8] = 0x60;
     sdata[9] = 0x60;
     sdata[10] = 0x00;
     sdata[11] = 0x00;
     sdata[12] = 0x3F;
     sdata[13] = 0x01;
     writeCmd(Idle, 0x0E,ch);
     readCmd(ch);
     
     sdata[0] = 0x03;
     sdata[1] = 0xA1;
     sdata[2] = 0x00;
     sdata[3] = 0xF8;
     sdata[4] = 0x01;
     sdata[5] = 0x18;
     sdata[6] = 0x00;
     sdata[7] = 0x20;
     sdata[8] = 0x60;
     sdata[9] = 0x60;
     sdata[10] = 0x00;
     sdata[11] = 0xFC;
     sdata[12] = 0x3F;
     sdata[13] = 0x01;
     writeCmd(Idle, 0x0E,ch);
     readCmd(ch);
     
     sdata[0] = 0x03;
     sdata[1] = 0xA1;
     sdata[2] = 0x00;
     sdata[3] = 0xF8;
     sdata[4] = 0x01;
     sdata[5] = 0x18;
     sdata[6] = 0x00;
     sdata[7] = 0x20;
     sdata[8] = 0x60;
     sdata[9] = 0x60;
     sdata[10] = 0x00;
     sdata[11] = 0x7C;
     sdata[12] = 0x3F;
     sdata[13] = 0x01;
     writeCmd(Idle, 0x0E,ch);
     readCmd(ch);
     
     sdata[0] = 0x03;
     sdata[1] = 0xA1;
     sdata[2] = 0x00;
     sdata[3] = 0xF8;
     sdata[4] = 0x01;
     sdata[5] = 0x18;
     sdata[6] = 0x00;
     sdata[7] = 0x20;
     sdata[8] = 0x60;
     sdata[9] = 0x60;
     sdata[10] = 0x00;
     sdata[11] = 0x3C;
     sdata[12] = 0x3F;
     sdata[13] = 0x01;
     writeCmd(Idle, 0x0E,ch);
     readCmd(ch);
     
     sdata[0] = 0x03;
     sdata[1] = 0xA1;
     sdata[2] = 0x00;
     sdata[3] = 0xF8;
     sdata[4] = 0x01;
     sdata[5] = 0x18;
     sdata[6] = 0x00;
     sdata[7] = 0x20;
     sdata[8] = 0x60;
     sdata[9] = 0x60;
     sdata[10] = 0x00;
     sdata[11] = 0x5C;
     sdata[12] = 0x3F;
     sdata[13] = 0x01;
     writeCmd(Idle, 0x0E,ch);
     readCmd(ch);
     
     sdata[0] = 0x03;
     sdata[1] = 0xA1;
     sdata[2] = 0x00;
     sdata[3] = 0xF8;
     sdata[4] = 0x01;
     sdata[5] = 0x18;
     sdata[6] = 0x00;
     sdata[7] = 0x20;
     sdata[8] = 0x60;
     sdata[9] = 0x60;
     sdata[10] = 0x00;
     sdata[11] = 0x6C;
     sdata[12] = 0x3F;
     sdata[13] = 0x01;
     writeCmd(Idle, 0x0E,ch);
     readCmd(ch);
     
     sdata[0] = 0x03;
     sdata[1] = 0xA1;
     sdata[2] = 0x00;
     sdata[3] = 0xF8;
     sdata[4] = 0x01;
     sdata[5] = 0x18;
     sdata[6] = 0x00;
     sdata[7] = 0x20;
     sdata[8] = 0x60;
     sdata[9] = 0x60;
     sdata[10] = 0x00;
     sdata[11] = 0x74;
     sdata[12] = 0x3F;
     sdata[13] = 0x01;
     writeCmd(Idle, 0x0E,ch);
     readCmd(ch);
     
     sdata[0] = 0x03;
     sdata[1] = 0xA1;
     sdata[2] = 0x00;
     sdata[3] = 0xF8;
     sdata[4] = 0x01;
     sdata[5] = 0x18;
     sdata[6] = 0x00;
     sdata[7] = 0x20;
     sdata[8] = 0x60;
     sdata[9] = 0x60;
     sdata[10] = 0x00;
     sdata[11] = 0x70;
     sdata[12] = 0x3F;
     sdata[13] = 0x01;
     writeCmd(Idle, 0x0E,ch);
     readCmd(ch);
    }

    RSing.9
    RSing.9Author
    Associate
    August 27, 2021

    int main(void)

    {

    nrf_gpio_cfg_output(SPI_CS[0]);

     nrf_gpio_cfg_output(SPI_CS[1]);

     nrf_gpio_cfg_output(SPI_CS[2]);

     nrf_gpio_cfg_output(SPI_CS[3]);

     nrf_gpio_cfg_output(SPI_CS[4]);

     nrf_gpio_cfg_output(SPI_CS[5]);

     nrf_gpio_cfg_output(SPI_CS[6]);

     nrf_gpio_cfg_output(SPI_CS[7]);

     nrf_gpio_cfg_output(SPI_CS[8]);

     nrf_gpio_cfg_output(SPI_CS[9]);

     SPI_init();

     nrf_gpio_pin_set(SPI_CS[0]);

     nrf_gpio_pin_set(SPI_CS[1]);

     nrf_gpio_pin_set(SPI_CS[2]);

     nrf_gpio_pin_set(SPI_CS[3]);

     nrf_gpio_pin_set(SPI_CS[4]);

     nrf_gpio_pin_set(SPI_CS[5]);

     nrf_gpio_pin_set(SPI_CS[6]);

     nrf_gpio_pin_set(SPI_CS[7]);

     nrf_gpio_pin_set(SPI_CS[8]);

     nrf_gpio_pin_set(SPI_CS[9]);

     nrf_delay_ms(100);

     reset_cr95hr(0);

     nrf_delay_ms(3);

     while (!EchoResponse(0));

     nrf_delay_ms(3);

     //Calibration(0);

     //nrf_delay_ms(3);

     IndexMod_Gain(0);

     nrf_delay_ms(3);

     AutoFDet(0);

     nrf_delay_ms(3);

     Select_ISO_IEC_14443_A_Protocol(0);

     nrf_delay_ms(3);

     //Clear_Screen(0);

     //string_display("ERR1", 2, 0);

     while(1){

      if (!TAG_Flag)

       GetNFCTag(0);                        // Get NFC ID

      if (!NFC_Flag)

       GetTagID(0);                        // Get Tag ID

      if (ID[0] == 0){                       // If there is no tag present

       flag++;                          // Increment counter flag

      }

      else {                            // If tag is present

       flag = 0;                         // Reset counter flag

       {                  // Compare previous and current tag ID

        //UART1_Write_Text("Tag ID:");

        //UART1_Write_Text(ID);

        //UART1_Write_Text("\r\n");

        ble_send("OK\r\n", strlen("OK\r\n"));

        strcpy(ID_old, ID);                   // Set current ID as previous ID

        nrf_delay_ms(100);     

       }

      }

      if(flag > 2){                        // If counter flag has reached value > 5

       //UART1_Write_Text("Put the Tag over the Antenna\r\n");

       ble_send("NOT\r\n", strlen("NOT\r\n"));

       ID_old[0]= 0;                       // Terminate the old ID string

       flag = 0;                         // Reset counter flag

      }

      ID[0]= 0;                          // Terminate the ID string

      // Clear read and write buffers

      for(j=0; j<18; j++){

       rdata[j] = 0;

       sdata[j] = 0;

      }

     }

    }

    Brian TIDAL
    Brian TIDALBest answer
    ST Technical Moderator
    August 27, 2021

    Hi,

    can you share more details about your hardware setup:

    • do you use your own custom board or do you use existing board (such as X-NUCLEO-NFC03A1 connected to an MCU board)
    • how is connected the CH95HF to the MCU: PCB connection or wire jumpers? If wire jumpers are used, verify them
    • what is the setup of the SSI_0 and SSI_1 pins? Can you probe those 2 signals during startup and make sure SSI_0=1 and SSI_1=0
    • can you check that the CR95HF is properly powered

    Regarding the startup sequence, before sending the ECHO sequence, can you send a poll command and check that bit 2 is set in the poll answer?

    Rgds

    BT

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.