Skip to main content
GLi.6
Associate
July 5, 2022
Solved

CR95HF Linux kernel driver

Hi,

I am working on linux kernel v4.19 to bring up the cr95hf via SPI, there is a existing driver called st95hf, I enabled it, and it can be probed. can get ECHO back.

when I used nfc neard to test the driver, it always gives errors like below:

[ 501.027260] spi_geni 988000.spi: Zero length transfer

[ 501.027307] st95hf spi1.0: SPI transfer failed: -22

[ 501.027393] spi_master spi1: failed to transfer one message from queue

[ 501.027436] st95hf spi1.0: spi_recv_resp, data read error = -22

[ 501.027471] st95hf spi1.0: spi error from st95hf_spi_recv_response(), err = 0xffffffea

[ 501.027506] nfc nfc0: protocol sel send field off, err = 0xffffffea

[ 501.036499] digital: digital_in_configure_hw: in_configure_hw failed: -22

[ 501.037971] spi_geni 988000.spi: Zero length transfer

[ 501.038042] st95hf spi1.0: SPI transfer failed: -22

[ 501.038181] spi_master spi1: failed to transfer one message from queue

[ 501.038246] st95hf spi1.0: spi_recv_resp, data read error = -22

[ 501.038298] st95hf spi1.0: spi error from st95hf_spi_recv_response(), err = 0xffffffea

[ 501.038351] nfc nfc0: protocol sel send field off, err = 0xffffffea

[ 501.048640] digital: digital_in_configure_hw: in_configure_hw failed: -22

[ 501.050030] spi_geni 988000.spi: Zero length transfer

[ 501.050090] st95hf spi1.0: SPI transfer failed: -22

I would like to know is there any verified cr95hf driver for linux kernel?

This topic has been closed for replies.
Brian TIDAL
Brian TIDALBest answer
ST Technical Moderator
July 22, 2022

Hi,

I confirm that the package Linux_RFAL_st25r95_v2.0.4.tar.gz properly compiles and runs on RPi3.

The SPI SS pin is managed by software as a GPIO. Make sure that the allocated pin is free to be used. If needed, reallocate the cs0_pin used by the HW to another pin (use dtoverlay spi0-1cs,cs0_pin=x in /boot/config.txt where x is an unused pin).

Again, I would recommend to probe the SPI SPI CLK/MOSI/MISO/CS + SSI0 + SSI1 + IRQ_IN and IRQ_OUT with a logic analyzer to see what is going wrong.

Note: st25r95_com_spi.c should not be modified (in particular, there should not be a dummy byte in the echo command).

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

15 replies

Brian TIDAL
Brian TIDALBest answer
ST Technical Moderator
July 22, 2022

Hi,

I confirm that the package Linux_RFAL_st25r95_v2.0.4.tar.gz properly compiles and runs on RPi3.

The SPI SS pin is managed by software as a GPIO. Make sure that the allocated pin is free to be used. If needed, reallocate the cs0_pin used by the HW to another pin (use dtoverlay spi0-1cs,cs0_pin=x in /boot/config.txt where x is an unused pin).

Again, I would recommend to probe the SPI SPI CLK/MOSI/MISO/CS + SSI0 + SSI1 + IRQ_IN and IRQ_OUT with a logic analyzer to see what is going wrong.

Note: st25r95_com_spi.c should not be modified (in particular, there should not be a dummy byte in the echo command).

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.