Skip to main content
duncan
Associate II
Sep 25, 2013 2:57 PM UTC
Solved

CR95HF error code 4

Posted on September 25, 2013 at 16:57

occasionally when I send a

 CR95HFDll_SendReceive 

command, I get error code 4 back. 5 I understand - the USB is not connected, so I simply reconnect, but 4 is a communication error. How can I recover from this in my program? (it does not matter whether a tag is there or now) as currently the only way I can do it is by resetting the computer or running the ST M24LRxx application.

#cr95hf #select-protocol
This topic has been closed for replies.
Anais GALLIGANI
Anais GALLIGANIBest answer
Visitor II
Sep 26, 2013 12:23 PM UTC
Posted on September 26, 2013 at 14:23

Hello,

Due to answer 4 or 5, it might be linked to the USB that has lost the control.

In the software, when you are connecting again the DEMO-CR95HF-A to the USB with the command   « reconnect »,  the DEMO-CR95HF-A is connected again to the computer.

 

The issue might be linked to the protocol selection  used (ISO 15693 protocol_select), has been lost.

You might try the procedure to “reconnect�? with a select protocol procedure in order to be sure the CR95HF is well configured.

I hope this might help you,

Best regards,

Have a nice day,

ST NFC/RFID Dynamic tag support

2 replies

Anais GALLIGANI
Anais GALLIGANIBest answer
Visitor II
Sep 26, 2013 12:23 PM UTC
Posted on September 26, 2013 at 14:23

Hello,

Due to answer 4 or 5, it might be linked to the USB that has lost the control.

In the software, when you are connecting again the DEMO-CR95HF-A to the USB with the command   « reconnect »,  the DEMO-CR95HF-A is connected again to the computer.

 

The issue might be linked to the protocol selection  used (ISO 15693 protocol_select), has been lost.

You might try the procedure to “reconnect�? with a select protocol procedure in order to be sure the CR95HF is well configured.

I hope this might help you,

Best regards,

Have a nice day,

ST NFC/RFID Dynamic tag support

duncan
duncanAuthor
Associate II
Oct 1, 2013 1:31 PM UTC
Posted on October 01, 2013 at 15:31

Hi there,

yes you are correct. resetting the protocol gets rid of the problem. Thanks for your help, it's really appreciated!