Skip to main content
Enrico Tmiello
Associate
June 19, 2018
Solved

CR95HF, 64 Bytes Frames

Posted on June 19, 2018 at 08:28

Hi, We are Using a CR95HF and we're trying to read a frame of 78 bytes with CR95HFDll_SendReceive but we get in return a 64 bytes frame with CRC and error code CCCCCC.

Is there a way to solve the problem of the limited 64 bytes frame when using USB for the CR95HF?

♯

?

♯

?

#cr9hf #64bytes
    This topic has been closed for replies.
    NFC/RFID Customer support
    ST Employee
    June 22, 2018
    Posted on June 22, 2018 at 17:17

    Standard use or 02A8 command doesn't change ISO15693 RF protocol configuration. The only adjustment you can try to improve tag answer reception is to use 100% modulation (CR95HFDLL_SELECT, 0109

    )

    instead of 10% (CR95HFDLL_SELECT, 010D). I suppose that '0045' is the expected data to be received. 8E00 is an answer from CR95HF IC, it means that the communication has noise and the tag answer cannot be decoded successfully, the coupling between tag & reader is not the better one. Also, I don't understand ,02a02d command.

    Best regards

    NFC/RFID ST support

    5 replies

    NFC/RFID Customer support
    ST Employee
    June 19, 2018
    Posted on June 19, 2018 at 11:56

    Hi Enrico,

    the last firmware revision of the STM32 embedded in the CR95HF board allows to send and receive up to 512 bytes.

    This improvement is managed by the DLL used on the PC side and the STM32 firmware from ths CR95HF board.This improvement is transparent for user and fully managed by the STM32/DLL.

    New DLL can be found in the last version of CR95HF PC SW (STSW-95HF001 v2.2.0): DLL revision 1.2 supports this improvement.

       

    http://www.st.com/content/st_com/en/products/embedded-software/st25-nfc-rfid-software/stsw-95hf001.html

    STM32 firmware can be download in our internet web site (STSW-M24LR007 v3.7.1):

       

    http://www.st.com/content/st_com/en/products/embedded-software/st25-nfc-rfid-software/stsw-m24lr007.html

    ST LINK V2 board can be used to update your M24LR-DISCOVERY board.

    http://www.st.com/content/st_com/en/products/development-tools/hardware-development-tools/development-tool-hardware-for-mcus/debug-hardware-for-mcus/debug-hardware-for-stm32-mcus/st-link-v2.html

    Best regards

    NFC/RFID ST support

    Enrico Tmiello
    Associate
    June 20, 2018
    Posted on June 20, 2018 at 07:54

    Hi, Thank you for the answer, the new firmware resolved the 94 bytes problem but reading and writing are a lot worse now, is there any parameter or configuration that might help us?

    NFC/RFID Customer support
    ST Employee
    June 20, 2018
    Posted on June 20, 2018 at 10:07

    HI,

    Can you please specify what is not working well ? The only différences between the previous software and the actual one is that, now, more than 1 USB transaction is used to be able to transfer more than 64 bytes (1 USB transaction for 64bytes, 2 for 94bytes). I don't know if you are using the CR95HF through the PC software or your own developed software. In case of own software, you have to know that, to enable big amount of data transfer(in iso15693 rf protocol, the cr95hf is configured as specific way. So when changing rf protocol from iso15693 to iso1443A for example, you need to add reset_spi commad between. All other rf setting are not changed.

    Best regards

    NFC/RFID ST support