Skip to main content
Associate
September 20, 2023
Solved

Continues data Transmission with i²c

Is it possible to transfer large data files, meaning bigger than the internal memory of the tag?

The intended purpose is to have a stm32 connected to an i²c dynamic tag and be able to write large files, like a new firmware, to the stm32 MCU. The problem is, that I couldn't find documentation if it is possible to simultaneously read the data via i²c which is currently written to the tag via NFC. If not possible in a continues stream, reading in chunks would be a viable alternative. As long as it is possible to do in one NFC "Session". That would allow a 0 port device that can be sealed towards the environment. 

This topic has been closed for replies.
Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
September 20, 2023

For example, you could look at the software package STSW-ST25DV001, which deals with this topic.

Good luck!
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

1 reply

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
September 20, 2023

For example, you could look at the software package STSW-ST25DV001, which deals with this topic.

Good luck!
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.