Confused about the 'load modulation' setting of CHIP_INIT configuration in ST25R3916 GUI and 'analogConfigTbl_NFC06A1.c'
- I loaded the MB11414-A_v1.xml into ST25R3916 Discovery GUI. And find there is a register '0x68', but in ST25R3916's datasheet, I can't find 0x68, only 0x28. Where 0x68 comes from.
- If it's a typo, that is 0x68 is actually 0x28, write 0x00 to mask 0x20 should disable the external load modulation, right? But the comment is 'Disable Internal Modulation', why ?
- Similar to above, write 0x10 to mask 0x10 should enable the internal load modulation, right? But the comment is 'use external load modulation'.
- In analogConfigTbl_NFC061A1.c, same problem exist there
Best regards.