Skip to main content
HStee.1
Associate
March 24, 2023
Solved

Cannot send larger chuncks than 4096 bytes to ST25DV64KC

We use dev. kit: ANT7-T-ST25DV64KC with app version: ST25NFCTap version V3.7.0 / ST25SDK: 1.10.0 public version. Q: I try to write binary data from file to it. I succeed in sending 4096 bytes. But when I try to send larger files it fails (tried 8192 bytes) with the error message:

Error while writing data:

com.st.st25sdk.STException: Error BAD_PARAMETER

Q: Is this a known issue or am I doing something wrong?

This topic has been closed for replies.
HStee.1
HStee.1Best answer
Associate
March 27, 2023

After doing some reading/writing tests over I2C I found the "problem" myself. The NFC tag concerned is of size 64k BITS. For some reasons (bad reading) I assumed 64k bytes. 64kbits results in 8kbytes and that is exactly what I can read/write to it.

2 replies

HStee.1
HStee.1AuthorBest answer
Associate
March 27, 2023

After doing some reading/writing tests over I2C I found the "problem" myself. The NFC tag concerned is of size 64k BITS. For some reasons (bad reading) I assumed 64k bytes. 64kbits results in 8kbytes and that is exactly what I can read/write to it.

Tesla DeLorean
Guru
March 27, 2023

FLASH and EEPROM memories have historically been quoted in BITs as this directly drives the size and number of transistors in the memory array.

The byte/word formats tend to be on the interface side, and can also vary widely, ie 4, 8, 16, 32, etc. With arrays within SoC the bus/line widths can also be significantly bigger as the bus doesn't need to be exported to pins on a package. On STM32 devices the array's are frequently 64 or 128-bit wide, so the initial fetch is quite expensive, but subsequent bytes are immediately available (zero time)

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..