Skip to main content
DJeon.4
Associate III
August 16, 2022
Solved

Can I use the card emulator function with the CR95HF V5 7BAHF V6 PHL 210 chip?

​Hello, I am implementing Card Emulation function with CR95HF Chip. There is no description of the card emulator function in the datasheet, so I'm not sure if it can be used or not.

If possible, can you provide the material in code form?

It is implemented with Arduino sketch program. I've asked the question a few times before, but I haven't been able to solve it. I would be very grateful if you could help me.

    This topic has been closed for replies.
    Brian TIDAL
    Brian TIDALBest answer
    ST Technical Moderator
    August 22, 2022

    Hi,

    the Card Emulation commands are defined in the ST25R95 datasheet.

    The X-CUBE-NFC3 package contains the RFAL framework and API for the support of Card Emulation feature but the low level driver (st25r95_com_ce.c file) for this feature is only provided on request.

    Regarding Arduino, there is an existing support of the X-NUCLEO-NFC03A1 (CR95HF/ST25R95 reader) in the stm32duino ecosystem but limited to the reader features (i.e. not providing Card Emulation support). See: https://github.com/stm32duino/X-NUCLEO-NFC03A1

    Rgds

    BT

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

    4 replies

    Peter BENSCH
    ST Technical Moderator
    August 16, 2022

    Yes, you can also realise card emulation with the CR95HF, examples can be found in the software package X-CUBE-NFC3.

    Does is answer your question?

    Regards

    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    DJeon.4
    DJeon.4Author
    Associate III
    August 17, 2022

    I use Arduino, so I can't find an example in the file you linked. Can you tell me where it is?

    Tesla DeLorean
    Guru
    August 17, 2022

    I don't think they were offered as Arduino examples, that's your platform of choice. You'll need to review the code/examples as provided and port them

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Brian TIDAL
    Brian TIDALBest answer
    ST Technical Moderator
    August 22, 2022

    Hi,

    the Card Emulation commands are defined in the ST25R95 datasheet.

    The X-CUBE-NFC3 package contains the RFAL framework and API for the support of Card Emulation feature but the low level driver (st25r95_com_ce.c file) for this feature is only provided on request.

    Regarding Arduino, there is an existing support of the X-NUCLEO-NFC03A1 (CR95HF/ST25R95 reader) in the stm32duino ecosystem but limited to the reader features (i.e. not providing Card Emulation support). See: https://github.com/stm32duino/X-NUCLEO-NFC03A1

    Rgds

    BT

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.