Skip to main content
smithderek2000
Associate III
May 19, 2023
Solved

Best way to test st25R3911B single ended configuration on a development board

Hello,

I'm working on a product that needs sixteen antennas, so we're looking at using the ST25R391x series but have it be single ended, with each output going to a 1:8 antenna MUX. I have the multiplexer to test but first need to get single ended operation working. What is the best way to do that on one of the STMicro eval boards? I saw this answer and also this app note AN5592 but their baseline differential component values were very different from the eval boards so it made me cautious.

Do you have a guide for which component values to change on one of the ST25R391x dev boards to allow for single ended operation? The end product uses a ST25R3916B but I have development boards for both the '3916B and the '3911. I don't have access to a network analyzer unfortunately.

Also, when testing the single ended implementation, do I need to remove all the components on the other channel? It looks like that was done in AN5592.

Finally, I think this antenna multiplexing would make for a great app note. I have it working with relays but want to use a silicon MUX instead. I can provide more information if it would help.

Thanks,

Derek

This topic has been closed for replies.
Carlo Corlattoni
Carlo CorlattoniBest answer
ST Employee
August 4, 2023

Hello,

the appnote AN5592 already describes which component values to use for a single ended configuration with STEVAL antenna. You would need to additionally disconnect the second antenna damping resistor and ground this antenna end. Then switch to one RFO driver (bit 7 and bit 6) in the IO Configuration register 1.

Regards,

 

1 reply

Carlo Corlattoni
Carlo CorlattoniBest answer
ST Employee
August 4, 2023

Hello,

the appnote AN5592 already describes which component values to use for a single ended configuration with STEVAL antenna. You would need to additionally disconnect the second antenna damping resistor and ground this antenna end. Then switch to one RFO driver (bit 7 and bit 6) in the IO Configuration register 1.

Regards,