Skip to main content
IBARH.1
Associate
January 27, 2020
Solved

An init error in the screen

Hello!

I want to test the ST25R3916 discovery kit so I download the software :Graphical User Interface. the device is well connected.However ,I see an error that appears on the screen when i connect the card. as a result I can not active the USB mode, I kept the user button pressed while I power/reset the matherboard.

I didin't succeed to connect the USB and the status turns always to red .

Can you help to solve the problem please !

Thank you .

    This topic has been closed for replies.
    Ulysses HERNIOSUS
    ST Technical Moderator
    January 28, 2020

    Hi Ines,

    I don't see any attachment. The motherboard has two different USB plugs: 1 mini-USB (ST-LINK USB) and 1 micro-USB (MCU USB). Communication with the GUI only works through micro plug: MCU-USB.

    Regards, Ulysses

    5 replies

    Ulysses HERNIOSUS
    ST Technical Moderator
    January 28, 2020

    Hi,

    please share more details:

    • Which exact board version do you have in hand?
    • Which USB plug on the board do you use?
    • Text / screenshot of error message
    • Content of the display of the board
    • Which card do you connect? Or do you mean the board?

    Regards, Ulysses

    IBARH.1
    IBARH.1Author
    Associate
    January 28, 2020
    Hi ,
    Thank you for answering . you will find two attachments which show my problem . Indeed as as I plug in the the mother card , an error appears on the screen . I check the stlink for this card through the device manager and it is well connected . In the GUI screen said that I have to press the user bottom and to RESET POWER in order to activate the USB mode but I didin’t succeed .I use USB cable version 2.0
    Best regards,
    Ines
    Ulysses HERNIOSUS
    ST Technical Moderator
    January 28, 2020

    Hi Ines,

    I don't see any attachment. The motherboard has two different USB plugs: 1 mini-USB (ST-LINK USB) and 1 micro-USB (MCU USB). Communication with the GUI only works through micro plug: MCU-USB.

    Regards, Ulysses