Skip to main content
ETann.1
Visitor II
February 24, 2023
Question

Adafruit ST25DV16K not able to write a link that has more than 24 characters using HelloWorld

I'm having a bit of trouble with my Adafruit st25dv16 and the HelloWorld library.

Specifically, I'm running into a problem when I try to write links that are longer than 24 characters.

I've noticed that I can write shorter links and read them just fine using my mobile device. However, whenever I try to read a link that's longer than 24 characters, I get a "null" message instead.

I was wondering if you might be able to offer some advice on how I can work around this issue. Do you know if it's possible to write longer links to the Adafruit st25dv16 using the HelloWorld library? Or maybe there are some other libraries or tools I could use instead?

This topic has been closed for replies.

3 replies

Schuyler
Associate III
March 14, 2023

是�?�有代�?�?编写和读�?�?

Ulysses HERNIOSUS
ST Technical Moderator
March 15, 2023

Translation:

"What is the difference between the two?"

parata.carlo
ST Employee
March 30, 2023

Hello @ETann.1​ ,

what is your hardware setup? Which HelloWorld library are you using? Please, could you provide more information about your hardware and software setup?

Best Regards,

Carlo