Skip to main content
DSai.1
Associate III
August 19, 2022
Solved

about IRQ pin in X-NUCLEO-NFC06A1

Dear Sir,

When I read the document of X-NUCLEO-NFC06A1, I found that the IRQ pin is not

connected to CN5. I wonder the demo sample provided in

ST25NFC_Embedded_Lib_ST25R3916_1.4.0\Projects\STM32L476RG-Nucleo\Applications\X-NUCLEO-NFC06A1 do not use IRQ interrupt?

best regards

Dai Sai

This topic has been closed for replies.
Brian TIDAL
Brian TIDALBest answer
ST Technical Moderator
August 22, 2022

Hi,

IRQ_MCU is by default routed to CN8.1.

CN5.2 is only an alternate routing (ST9 is open in the factory configuration).

See Table 1 in UM2615.

ST25NFC_Embedded_Lib_ST25R3916_1.4.0\Projects\STM32L476RG-Nucleo\Applications\X-NUCLEO-NFC06A1 uses IRQ_MCU on CN8.1/PA0

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

2 replies

Brian TIDAL
Brian TIDALBest answer
ST Technical Moderator
August 22, 2022

Hi,

IRQ_MCU is by default routed to CN8.1.

CN5.2 is only an alternate routing (ST9 is open in the factory configuration).

See Table 1 in UM2615.

ST25NFC_Embedded_Lib_ST25R3916_1.4.0\Projects\STM32L476RG-Nucleo\Applications\X-NUCLEO-NFC06A1 uses IRQ_MCU on CN8.1/PA0

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
DSai.1
DSai.1Author
Associate III
August 23, 2022

Dear Brian,

thank you for your reply.

I got it.

best regards

Dai Sai