Skip to main content
uilter
Senior
June 6, 2023
Solved

How setup LTDC to DE MODE

  • June 6, 2023
  • 20 replies
  • 16529 views

Hi,

My MCU is a STM32H753BIT6. This is a custom board that works fine with SYNC-MODE displays types.

I have a new display only works in DE MODE. It not requires the HSYNC or VSYNC signals.

Is there any way to configure LTDC peripheral and TouchGFX to work only in DE MODE? This is a communication image about this mode.


_legacyfs_online_stmicro_images_0693W00000bVejGQAS.png 

I disconnect physically the VSYNC/HSYNC signals and ground it to make sure.

Thanks for any tip and help!

This topic has been closed for replies.
Best answer by uilter

It works =)

I change the settings to:


_legacyfs_online_stmicro_images_0693W00000bVjksQAC.png 

Also I reconnect the VSYNC and HSYNC signals to LTDC peripheral. Without it the display keep dead.

Just after these modifications that I mentioned it worked.

I had some flickers in transaction screen and animation widgets, but reducing a little bit the LTDC_CLK it works well. (Fine tuning)

@ktrofimo​ thanks to help me with it.

20 replies

ktrofimo
Senior III
June 6, 2023

What is your display model? Do you have datasheet? I would start with comparing "hsync/vsync" and "de only" waveforms...

uilter
uilterAuthor
Senior
June 6, 2023

I can not upload the file here, just some prints.

This is the timming table


_legacyfs_online_stmicro_images_0693W00000bViUPQA0.png
_legacyfs_online_stmicro_images_0693W00000bViUZQA0.png 

Resumed pinout: note there is not VSYNC and HSYNC


_legacyfs_online_stmicro_images_0693W00000bViUoQAK.pngThen my CubeMX setup (My LTDC clock is 25MHz):


_legacyfs_online_stmicro_images_0693W00000bViV8QAK.png 

Let me know if you need more informations.

Thanks.

ktrofimo
Senior III
June 6, 2023

What about display model? According to information you posted here it should work as regular TFT just without HSYNC and VSYNC signals. If you can't publish document - just give a model and/or link to the datasheet.

INaee.1
Associate II
June 8, 2023

Hi .

I am using both type of TFTs ( with VSync + HSync + DE ) and also DE mode only

you dont need to disconnect the connection of VSync & HSync for DE Mode.

Just put the value 1 for each i-e VSync =1 & HSync = 1 in CubeMX

these values always -1 of actual value , that means 1-1 = 0 >> DE Only Mode.

I hope this will work

BTW ,, my custom design board is across H745xit6 with 7inch RGB TFT of 1024X600 resolution and I am running TouchGFX very well on it.

Imran

uilter
uilterAuthor
Senior
June 8, 2023

Hi @Community member​ 

Thanks fot your comment.

When you sad "put the value 1 for each i-e VSync =1 & HSync = 1 in CubeMX" is set the polarity in LTDC configuration to Active HIGH or set the GPIOs to output and config it to HIGH state?

Thanks.

INaee.1
Associate II
June 8, 2023

Hi

my experience is ....

You can't disable the LTDC essential signals and set as gpio output , if you do so then whole LTDC becomes inactive in cubemx.

 

The Vsync & Hsync signals can be disabled by putting value 1 for each , as I mentioned before and practically observed.

 

BTW .. my most recent TouchGFX experiment with custom designed board is across STM32H745XIT6 Core board with 1024X600 Chinese TFT .

INaee1_0-1687543529986.jpeg

INaee1_1-1687543529991.jpeg

The above board is with multiple communication protocols . and this customized board is based on following Core Board.

 H9f2461e93d6d46a2b2c3b57bd4dd4faaw.jpg_640x640Q9.jpg

I also implemented Modbus Master RTU with TouchGFX on my previous development board.

Simulated the Modbus values from ModBusSlave utility on laptop and observed values on TouchGFX in numeric figures , custom guages & vertical bars.

 

 

thanks

 

 

INaee.1
Associate II
June 8, 2023

Moreover ,,

I am using touchGFX on following TFT resolutions

5inch 1280X720 .. RGB + Spi (Generic Chinese Cellphones)

7inch 800X480 .. RGB (Generic Chinese)

7inch 1024X600 .. RGB (Generic Chinese)

7inch 1024X600 .. LVDS (Samsung Tab3)

and many more from LCD Monitors (LVDS type TFTs )

1024X600

1280X800

etc ..

uilter
uilterAuthor
Senior
June 8, 2023

In this custom board I also is with another two displays:

  • 7inch 1024X600
  • 10.1inch 1024X600

Next step I will design a RGB->LVDS bridge to a bigger display with high resolution (1280x800).

In another custom board I put a RGB->HDMI bridge. I not test it yet.

INaee.1
Associate II
June 11, 2023

Hi ..

Here is TouchGFX running on HP S1932 18.5" Monitor's LVDS LCD with 1366x768 resolution .

The lcd part no. is LTM185AT04 or Equivalent . The driver is stm32f429i-discovery + sn75lvds83b  


_legacyfs_online_stmicro_images_0693W00000dDV59QAG.png
_legacyfs_online_stmicro_images_0693W00000dDUzSQAW.pngBTW ,, I tested ThinkPad T400 TFT 1280x800 resolution with my RGB>LVDS and working fine.

ktrofimo
Senior III
June 8, 2023

About 10 years ago I have tested RGB->HDMI bridge (I believe it was from TI) and it was working fine in HD mode (720p) because STM32F429 was too slow for FHD (1080p). But RGB->CVBS (Analog Devices, composite TV) bridge test failed because I was unable to output 27MHz clock (doubled and sync'ed with pixelclock 13,5MHz)

uilter
uilterAuthor
Senior
June 8, 2023

FYI

I'm using the TFP410PAP from TI for RGB-HDMI bridge.

Associate II
February 14, 2024

I tried adjusting display settings and display works!.