Skip to main content
ARied.1
Associate
July 21, 2022
Solved

How to install Atollic TRUEStudio on Linux?

  • July 21, 2022
  • 5 replies
  • 3732 views

Hello, I have installed previous version of Atollic (< 9.3) before following the official installation guide, but now it seems to be outdated since the downloadable file isn't a .tar.gz file anymore, but now just a .gz file.

I am using EndeavourOS Linux x86_64. I have tried doing gzip -d en.TrueSTUDIO_V9.3_lin.gz, but then I don't know what to do with the extracted file. I mean, it extracts a en.TrueSTUDIO_V9.3 file which I tried to make executable with chmod +x, but nothing happens. If I open the directory with thunar, I can see the previous file as a compressed file which stills has another file inside. Nonetheless, I cannot decompress said file.

I would appreciate any assistance.

Thank you in advance.

This topic has been closed for replies.
Best answer by mattias norlander

Hi @ARied.1​ ,

Sorry for the delay. Just arrived back to office after summer holiday.

Try renaming the installer from blabla.gz to blabla.tar.gz

I only have access to a Windows machine but with 7-zip I can extract the expected files by renaming the file...

Then the next question is - why has this old file which has not been modified for years been renamed on the delivery server?! <-- This I will have to check internally. Sounds like IT-issue.

5 replies

raptorhal2
Lead
July 21, 2022

@mattias norlander​ is probably the best expert, providing he is not on vacation.

Cheers, Hal

Andrew Neil
Super User
July 22, 2022

TRUEStudio is Not Recommended for New Designs (NRND) - STM32CubeIDE is the replacement:

0693W00000QLsSoQAL.png 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Nikita91
Lead II
July 22, 2022

I understand that we prefer to use TrueSTUDIO, it is also my case.

It's faster, reliable, and and it's also upgadable: How to update TrueSTUDIO and some tips to configure Eclipse based IDE. - AdAstra-Soft

But here I can't help because I'm a Windows user...

ARied.1
ARied.1Author
Associate
July 22, 2022

@Andrew Neil​ I understand, but it has been chosen as the IDE for a class I'm in, so I can't really do anything about it. Right now I'm running it on a WM with Windows, but it's really not ideal, so I wanted to know if there is any solution.

Andrew Neil
Super User
July 22, 2022

@ARied.1​ "it has been chosen as the IDE for a class I'm in"

The you should go to the teacher for assistance - she must know how to do it.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
mattias norlander
ST Employee
August 10, 2022

Hi @ARied.1​ ,

Sorry for the delay. Just arrived back to office after summer holiday.

Try renaming the installer from blabla.gz to blabla.tar.gz

I only have access to a Windows machine but with 7-zip I can extract the expected files by renaming the file...

Then the next question is - why has this old file which has not been modified for years been renamed on the delivery server?! <-- This I will have to check internally. Sounds like IT-issue.

ARied.1
ARied.1Author
Associate
August 11, 2022

Yep, this worked!! Thank you very much!