Skip to main content
LROCH.11
Associate II
June 28, 2021
Solved

I have create a project to communicate via a fdcan bus on stm 32h723zgt microcontroller but i have no interrupt generated

  • June 28, 2021
  • 7 replies
  • 3077 views

i have connected the tx pin to rx pin on fbcan3 interface

you will find my project in attacheement

thanks

This topic has been closed for replies.
Best answer by mƎALLEm

Hello,

Using nucleo-H723ZG board: to use CAN with this board you have either:

- Use FDCAN in loopback mode not in normal mode (which is your current config). The CAN cannot be handled as UART or SPI it has same specificity like arbitration, error management etc.. this arbitration is done when at least two nodes are connected via CAN bus through transceivers (normal mode).

In loopback mode, this arbitration mode is managed internally in the cell. so Rx and Tx pins are connected internally in the chip. refer to RM0468 rev2 page 2524/2524: External and internal loop back modes 

For loopback mode example, please refer to the example provided under: \Projects\STM32H743I-EVAL\Examples\FDCAN\FDCAN_Loopback

- Use FDCAN in normal mode but you have to add an external transceiver to connect your board to another CAN node through CAN bus (differential mode). You can use For example FDCAN2/FDCAN3 in normal mode but you have to add a transceiver for each one.

But at the same time you have to select the correct transceiver: classic mode which reaches 1Mb/s and FDCAN: it depends on what bitrates you will use.

For the clock, for loopback mode you may not encounter communication issues, but in normal mode you will. So for your design you have to an external precise crystal. For example you can use the clock source provided by ST-Link (8MHz) in bypass mode.

STM32

7 replies

mƎALLEm
ST Technical Moderator
June 28, 2021

Hello,

  • Could you please tell us what is the HW used? is it an ST board (Nucleo/Disco/Eval)? or something custom?
  • What do you mean by "i have connected the tx pin to rx pin on fbcan3 interface", did you connect FDCAN3_Tx to FDCAN3_Rx using a wire?
  • Just to note that it's not recommended to use HSI for CAN communication, please use an external precise crystal with RCC HSE config.

STM32

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
LROCH.11
LROCH.11Author
Associate II
June 28, 2021

Hello,

  • I used the nucleo-H723ZG board.
  • Yes, I connected a FDCAN3_Tx and FDCAN3_Rx  with a wire.
  • in my design i used the hsi clock

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
June 28, 2021

Hello,

Using nucleo-H723ZG board: to use CAN with this board you have either:

- Use FDCAN in loopback mode not in normal mode (which is your current config). The CAN cannot be handled as UART or SPI it has same specificity like arbitration, error management etc.. this arbitration is done when at least two nodes are connected via CAN bus through transceivers (normal mode).

In loopback mode, this arbitration mode is managed internally in the cell. so Rx and Tx pins are connected internally in the chip. refer to RM0468 rev2 page 2524/2524: External and internal loop back modes 

For loopback mode example, please refer to the example provided under: \Projects\STM32H743I-EVAL\Examples\FDCAN\FDCAN_Loopback

- Use FDCAN in normal mode but you have to add an external transceiver to connect your board to another CAN node through CAN bus (differential mode). You can use For example FDCAN2/FDCAN3 in normal mode but you have to add a transceiver for each one.

But at the same time you have to select the correct transceiver: classic mode which reaches 1Mb/s and FDCAN: it depends on what bitrates you will use.

For the clock, for loopback mode you may not encounter communication issues, but in normal mode you will. So for your design you have to an external precise crystal. For example you can use the clock source provided by ST-Link (8MHz) in bypass mode.

STM32

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
LROCH.11
LROCH.11Author
Associate II
June 28, 2021

hi,

can i use the interrupt in loopback mode?

mƎALLEm
ST Technical Moderator
June 28, 2021

Hello,

Yes of course, for Tx & Rx.

STM32

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
LROCH.11
LROCH.11Author
Associate II
June 29, 2021

hello

i just change in loopback mode in cube mx and i d'nt have any interrupt.

mƎALLEm
ST Technical Moderator
June 29, 2021

Hello,

Please refer to one of the following examples provided in STM32H7Cube which are using Rx interrupts:

\Projects\STM32H743I-EVAL\Examples\FDCAN\FDCAN_Classic_Frame_Networking

\Projects\STM32H743I-EVAL\Examples\FDCAN\FDCAN_Com_IT

The interrupt config is the same either in loopback or normal mode.

STM32

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.