Skip to main content
Duy Tran
Associate III
Mar 31, 2020 8:58 AM UTC
Question

STM32 USB CDC receiving more than 64 bytes

Hello,

I am using the USB CDC of NUCLEO-F767ZI board. MY firmware can transmit and receive OK through the USB CDC. However, I cannot receive more than 64 bytes, only the first 64 bytes are received. The transmission is OK, it can send more than 64 bytes.

I tested with Hercules, Tera Term, Putty and the results are the same.

Do you have any idea what I missed or did I do anything wrong?

Thanks and best regards,

Duy

This topic has been closed for replies.

16 replies

Pavel A.
Mar 31, 2020 9:34 AM UTC

Same issue as in this question. Looks like bug.

-- pa

Duy Tran
Duy TranAuthor
Associate III
Mar 31, 2020 1:51 PM UTC

Still debugging but no idea why. I tried different COM port software also.

ST Technical Moderator
Apr 2, 2020 4:12 PM UTC

Hello,

Which firmware package are you using ?

I will raise this internally for check and come back to you soon.

Best Regards,

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Duy Tran
Duy TranAuthor
Associate III
Apr 2, 2020 5:07 PM UTC

Hello Imen,

Thanks for your feedback, I am using STM32Cube_FW_F7_V1.16.0.

Best regards,

Duy

ST Technical Moderator
Apr 2, 2020 4:45 PM UTC

Could you please use the provided USB CDC application available on the Firmware package ? we are not expecting to run into this issue using cube firmware.

Then, please keep us about your progress on this.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Duy Tran
Duy TranAuthor
Associate III
Apr 2, 2020 5:09 PM UTC

I don't see any example using CDC alone for the Nucleo-F767ZI. If possible, can you provide me the one you are testing?

Thanks.

ST Technical Moderator
Apr 2, 2020 5:12 PM UTC

You may get inspired and re-use sections from the CDC example available on Eval project.

Are you using STM32CubeMX in your own project ?

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Duy Tran
Duy TranAuthor
Associate III
Apr 6, 2020 9:10 AM UTC

Yes I am using STM32CubeMX and STM32CubeIDE in my project, still porting the example and make it run on my Nucleo.

ST Technical Moderator
Apr 6, 2020 6:31 PM UTC

Hi @Duy,

Please share your ioc file, this will help our CubeMX team to check and analyze your issue.

Best Regards,

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Duy Tran
Duy TranAuthor
Associate III
Apr 7, 2020 6:23 PM UTC

Hello Imen,

Thanks for your offer, it is so kind of STMicro Support team.

Please see attached file.

Thanks and best regards,

Duy

ST Technical Moderator
Apr 9, 2020 5:41 PM UTC

Hello,

We confirm that the issue on STM32CubeMx side.

The function CDC_Receive_FS() doesn't use the Len parameter:

static int8_t CDC_Receive_FS(uint8_t* Buf, uint32_t *Len)
{
 /* USER CODE BEGIN 6 */
 USBD_CDC_SetRxBuffer(&hUsbDeviceFS, &Buf[0]);
 USBD_CDC_ReceivePacket(&hUsbDeviceFS);
 return (USBD_OK);
 /* USER CODE END 6 */
}

So, using USB CDC cannot receive more than 64 bytes and only the first 64 bytes are received.

This issue is raised internally for fix.

Best Regards,

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Duy Tran
Duy TranAuthor
Associate III
Apr 10, 2020 2:40 AM UTC

Hello Imen,

Thanks for your feedback. BTW, will it be available in the next version of SDK?

Will there any temporary fix at the moment?

Best regards,

Duy

ST Technical Moderator
Apr 10, 2020 8:25 AM UTC

Hello @Duy Tran​ ,

Sorry Duy Tran, after more investigation with CubeMx team, it appears that it's no a bug inside CubeMx tool:

static int8_t CDC_Receive_FS(uint8_t* Buf, uint32_t *Len)

as it's made a callback reception from the stack and the data received is in Buf, the length of the data is in Len, So, it's up to the user to use it.

So, this is a pure CubeMx generation, and CubeMX gives just and entry point and can't

generate the full application, the Core code of CDC_Receive_FS() is

well protected by user tags, this can not be considered as a generation issue.

So it is up to you to complete, change the application code.

Best Regards,

Imen

Best Regards,

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks