Skip to main content
HMora.1
Associate II
February 15, 2020
Question

Can't Receive Ethernet packets in STM32H750VB

Hi all,

I have used the Ethernet in my custom design board based on STM32H750VB and using STM32CubeIDE with the latest updates. It has an RMII connection to a PHY and I could successfully send UDP packets to the PC both with both polling and interrupt based methods. Unfortunately, I can't receive any packet from PC. Below are my observations:

  1. I am sure that PC is sending UDP broadcast packets because I see them on the Wireshark!.
  2. I have also seen that RXD[1:0] and CRS_DV signals are toggling and connected to the Microcontroller. hence there is not any problem with the PHY chip (LAN8742A).
  3. I have also configured the filters to pass all broadcast messages and every other filter settings to make sure that nothing is filtered in any layer.
  4. When I connect cable and immediately after initialization I see that MTLQICSR register changes to a state that shows receive overflow in MTL buffer happened and also MTLRQDR register shows that RX Queue is half or Full!. This happens even if I activate filters of MAC!. This is kind a strange because when all filters are nabled MAC should only pass specific packets to MTL!. while I am not sending any packets.

Regarding above descriptions I don't know why no packet is received or why HAL_ETH_IsRxDataAvailable() function can't find any received message.

I have also some questions I don't know why the automatic generated code doesn't use or initialize Rx_Buff array? Isn't it needed for the polling or interrupt mode?

I would really appreciate any help on this issue.

Thanks in advance,

Hossein

This topic has been closed for replies.

4 replies

alister
Senior III
February 16, 2020

Perhaps HAL_ETH_Start_IT hasn't been called.

Check out https://community.st.com/s/question/0D50X0000C6eNNSSQ2/bug-fixes-stm32h7-ethernet too.

HMora.1
HMora.1Author
Associate II
February 17, 2020

Hi alister,

Thanks for your reply. At least someone is here to answer what ST have not done in their drivers!. That's a shame!. However, I have called HAL_ETH_Start_IT as well. I have also tried your mentioned changes in that post. Below are my main modifications:

  1. I have replaced two files completely from your modified ones(stm32h7xx_hal_eth.c & stm32h7xx_hal_eth.h).
  2. I am not using D-Cache.
  3. I am not using a middleware like FreeRTOS, it is a simple standalone project none of polling or interrupt modes are receiving. but, I do not have problem in TX side.
  4. Once I tried to configure MPU for the start address of Ethernet - 0x30040000 - and tried to protect 32KB which covers all RX/TX buffers. It did not work. Then I replaced your MPU configuration that I don't know why you have used two regions starting from 0x30040000!. - can't realize differences between these two regions. After these modifications now I see that HArdFault_Handler() happens immediately in the _ETH_Start() function that you have added HAL_ETH_BuildRxDescriptors() at the beginning of that.
  5. I have to also add that I don't know where in stm32h7xx_hal_conf.h file I have to add those new defines and include statements:

/* Prevent "..\..\Core\Inc\stm32h7xx_hal_conf.h" from including stm32h7xx_hal_eth.h */

#define STM32H7xx_HAL_ETH_H

#include "..\..\Core\Inc\stm32h7xx_hal_conf.h"

/* Fix incorrectly-configured ETH macros */

#undef ETH_TX_DESC_CNT

#undef ETH_RX_DESC_CNT

#define ETH_TX_DESC_CNT 16

#define ETH_RX_DESC_CNT 16

/* Add not-yet-configured ETH macros */

#define ETH_PMT_IT_ENABLED 0

#define ETH_EEE_IT_ENABLED 0

#define ETH_EXTI_IT_ENABLED 0

/* Include stm32h7xx_hal_eth.h properly */

#undef STM32H7xx_HAL_ETH_H

#include "stm32h7xx_hal_eth.h"

Once again thanks for your help,

Hossein